Skip to main content
Batuhan A.
Associate III
Jun 4, 2021 12:10 PM UTC
Solved

I2C Bus pull-up resistor for multiple slave devices

Hello,

I am using multiple different sensors which require different pull-up resistors. For I2C BUS, I have to use just one pull-up resistor value for all sensors. How can I calculate or decide the resistor value?

MCU is STM32WB55.

Sensors are VL53L3CXV0DH and LSM6DSOTR.

Thank you,

Batuhan

This topic has been closed for replies.
LMI2
LMI2Best answer
Senior III
Jun 4, 2021 2:31 PM UTC

No, your sensors do not require different pull up values. Pull up resistor in I2C bus has to charge bus capacitances fast enough. And every chip must be able drive the bus/pull-up down.

Pull up resistor depends on how much capacitance your bus has =its lenght. And how many devices there are on the bus. You should check what is weakest chip on your, don't use lower resistor than that.

You need pull ups for both Sda and Scl.

Try 5k.

4 replies

LMI2
LMI2Best answer
Senior III
Jun 4, 2021 2:31 PM UTC

No, your sensors do not require different pull up values. Pull up resistor in I2C bus has to charge bus capacitances fast enough. And every chip must be able drive the bus/pull-up down.

Pull up resistor depends on how much capacitance your bus has =its lenght. And how many devices there are on the bus. You should check what is weakest chip on your, don't use lower resistor than that.

You need pull ups for both Sda and Scl.

Try 5k.

Tesla DeLorean
Guru
Jun 4, 2021 3:12 PM UTC

Usually a function of how long the connectivity is and how fast you plan on driving things. It everything is on a single board, with close proximity it's going to be a lot easier than having lots of board, hung off lots of cables. Also how much sink current the OD transistors on the I2C slave(s) expect to be sinking.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LMI2
Senior III
Jun 4, 2021 6:11 PM UTC

And you can check with an oscilloscope if all signals square and go from 0V to +VDD.

Batuhan A.
Associate III
Jun 7, 2021 6:15 AM UTC

Thank you for your replies @LMI2​ and @Community member​ 

They help me understand the topic.

Best regards