Skip to main content
PTHOM.1
Visitor II
March 29, 2022
Question

I would like to know if the limit of 104 sample/sec of Output Data Rate for Machine Learning Core and Finite State Machine embedded MEMS processing, can be raised to handle dynamic signal in industry, at the expense of higher consumption.

LSM6DSOX Inertial module handles linear acceleration output data rate up to 6667 Hz, while limit for MLC and FSM is 104 Hz.

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
March 31, 2022

Hi @PTHOM.1​ ,

unfortunately the limit of this ODR=104Hz cannot be overcome in the LSM6DSOX/RX family, since its clock/logic is shared also with the sensor hub, which can be synchronized with the accelerometer/gyroscope data-ready signal up to 104 Hz.

Next generation IMU sensors with ISPU, such as LSM6DSO16IS, will be capable of much higher ODRs (and more complex functions).

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon