Skip to main content
KKS
Associate II
August 14, 2018
Question

I want to get gps information using p nucleo lrwan1.

I want to get gps information using p nucleo lrwan1. Can I get an open source that can help? I'll use the uart port.(gps)

    This topic has been closed for replies.

    1 reply

    August 14, 2018

    Hello,

    I am afraid this is not possible. LoRa operates in EU at 868 MHz and 915 MHz in the US. However, GPS utilizes 1575.42 MHz (10.23 MHz × 154) called L1 and 1227.60 MHz (10.23 MHz × 120), called L2.

    David