Skip to main content
EYao.1
Visitor II
November 26, 2020
Question

I want check if Datecode 711D4 is year 2017 12 week. Please help check and reply me Thanks very much.

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    November 26, 2020

    Hi @EYao.1​ ,

    I can reply here since it might be of interest for other users.

    Which product are you using?

    Please note that, in general, the Datecode can be decoded as follows: 711D4

    • "7" means 2017
    • "11" means wk 11 2017
    • "D4" is the product code

    So basically your product has been assembled (and the marking printed) in wk11, but the lot name is given by the test week, that could be wk12 in your case, so your guess should be effective.

    -Eleon