Skip to main content
JBonn
Associate III
Mar 30, 2025 6:47 PM UTC
Question

I need SPI 5-wire interface code for the STM32L476 with the LSM303AGR

Basic function is to calculate Heading 25 times per second.

Using C++, STMCubeMX, and STM32L476IDE.

Chip is the STM32L476RET.  Is this chip fast enpough?

Need heading 25 times per second for main loop processing. Using timer 3.

HAL is working, but is much to slow.

Do not know how much faster LL would  be.

Code below for the Mag.

void Get_Mag (void); // Gets Mag, MagF, MagFG

// 1. Reads Mag x,y,z

// 2. Converts to 16 bits,

// 3. Converts to floating Point,

HAL_GPIO_WritePin(GPIOC,GPIO_PIN_5,GPIO_PIN_SET); // Sets Mag CS On

HAL_GPIO_WritePin(GPIOC, GPIO_PIN_4,GPIO_PIN_RESET); // Sets XL CS Off

TX[0] = (OUTX_L_REG_M | 0x80);

Mag_Data[0] = 0;

HAL_SPI_TransmitReceive(&hspi1,&TX[0],&Mag_Data[0],7,100);

TX[0] = (OUTX_H_REG_M | 0x80);

Mag_Data[1] = 0;

HAL_SPI_TransmitReceive(&hspi1,&TX[0],&Mag_Data[1],4,100);

TX[0] = (OUTY_L_REG_M | 0x80);

Mag_Data[2] = 0;

HAL_SPI_TransmitReceive(&hspi1,&TX[0],&Mag_Data[2],2,100);

TX[0] = (OUTY_H_REG_M | 0x80);

Mag_Data[3] = 0;

HAL_SPI_TransmitReceive(&hspi1,&TX[0],&Mag_Data[3],2,100);

TX[0] = (OUTZ_L_REG_M | 0x80);

Mag_Data[4] = 0;

HAL_SPI_TransmitReceive(&hspi1,&TX[0],&Mag_Data[4],2,100);

TX[0] = (OUTZ_H_REG_M | 0x80);

Mag_Data[5] = 0;

HAL_SPI_TransmitReceive(&hspi1,&TX[0],&Mag_Data[5],2,100);

HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5,GPIO_PIN_RESET); // Sets Mag CS Off

// I know the six reads could be done with one read.

// *********** Convert to 16 bits *************************************

Magx = (Mag_Data[1] << 8) + Mag_Data[0]; // Combine high and low

Magy = (Mag_Data[3] << 8) + Mag_Data[2];

Magz = (Mag_Data[5] << 8) + Mag_Data[4];

MagxF = Magx; // Convert to floating point

MagyF = Magy;

MagzF = Magz;

MagxFG = Magx * 0.061; // Convert to mg in floating point

MagyFG = Magy * 0.061;

MagzFG = Magz * 0.061;

} // End of Get Mag

void Get_XL (void); // Gets Ax, kk, AxFG, AxAxFG is similar to Get_Mag

 

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Apr 1, 2025 10:21 AM UTC

Please see How to insert source code.

What do you mean by SPI five-wire ?

 


@JBonn wrote:

Need heading 25 times per second


Should be entirely doable. How many bytes per second is that?

 


@JBonn wrote:

HAL is working, but is much to slow.

Do not know how much faster LL would  be.


So start by finding what, exactly, is making your HAL-based code so slow.

Why do you read just 1 byte at a time?

Why not do a single 6-byte transaction?

 

PS:

Did you look at the software ST provides:

https://www.st.com/en/mems-and-sensors/lsm303agr.html#tools-software

 

The datasheet shows a four-wire interface:

AndrewNeil_0-1743503171409.png

https://www.st.com/resource/en/datasheet/lsm303agr.pdf#page=16

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.