Skip to main content
VB.4
Associate II
March 24, 2022
Question

I have NUCLEO-L053R8. Now I need to interface LSM9DS1 directly with NUCLEO-L053R8 for testing using MotionFX Library. Is it possible to interface LSM9DS1 to test using MotionFX library? If Yes, Please suggest proper procedure/steps. Thank you.

..

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
April 8, 2022

Hi @VB.4,

you can start from the C GIthub examples for the LSM9DS1 device (lsm9ds1_read_data_polling.c), changing the hardware connection for the Vdd / SPI physical lines (from the NUCLEO_F411RE to the NUCLEO-L053R8), and then you can add the MotionFX Library to your project, taking as reference the examples of the X-CUBE-MEMS1 that you can find in the \Projects\STM32L073RZ-Nucleo\Applications\CUSTOM folder.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

-Eleon