Skip to main content
YBend.1
Associate III
October 17, 2022
Question

I have hand soldered a an ASM330LHHXTR 6DOF MEMS IMU onto a breakout board and need to verify whether the IC is working or not. Can someone please suggest how can I check if it is working perfectly. Thank you!!

..

    This topic has been closed for replies.

    3 replies

    KnarfB
    Super User
    October 17, 2022

    Presuming that the power consumption and supply voltages are reasonable,a next test could be reading the WHO_AM_I register and later some RW registers for testing the interface.

    hth

    KnarfB

    YBend.1
    YBend.1Author
    Associate III
    October 17, 2022

    Thanks KnarfB,

    Will try that out first.

    YBend.1
    YBend.1Author
    Associate III
    October 28, 2022

    Hey KnarfB,

    Tried reading the WHO_AM_I register with address 0x0F, however 0x6B which is its fixed value is not returned. The Arduino code that I have written is:

    #include <SPI.h>
     
     
    const int slaveSelectPin = 10;
     
    void setup() {
     Serial.begin(115200);
     // set the slaveSelectPin as an output:
     pinMode (slaveSelectPin, OUTPUT);
     // initialize SPI:
     SPI.begin(); 
    }
     
    void loop() {
     byte result;
     
     // Begin a read or write cycle
     digitalWrite(slaveSelectPin, LOW); //Enable the slave
     
     // Send the command to read register 0
     SPI.transfer(0x0F);
     
     // Now read a byte from the chip. THE VALUE WE SEND MAKES NO DIFFERENCE WHEN READING.
     // We just need to generate 8 clock pulses and sample the MISO line to get the data.
     // Sending a byte will generate the clock pulses
     //result = SPI.transfer(0x42); 
     
     // Register read operation complete
     digitalWrite(slaveSelectPin, HIGH); 
     
     Serial.print("WHO_AM_I register contains 0x");
     Serial.println(result,HEX);
     
     delay(1000);
    }

    I also debugged using a logic analyzer, however the MISO line does returns 0XFF.

    From these results, would it be advisable to conclude that there is an issue on the hardware front.

    Thank you very much !!