Skip to main content
QAbba.1
Associate II
February 17, 2022
Question

I have edited the real-time 'DataLog' application provided in STSW-STLKT01_V2.5.0 to include the MotionDI_update function. However, my code hangs after I get the tilt and acceleration values for the first time. How to solve this?

int main(void)
{
	
 HAL_Init();
 
 /* Configure the System clock to 80 MHz */
 SystemClock_Config();
	
	MX_GPIO_Init();
	MX_DMA_Init();
 
 MX_CRC_Init();
	MX_RTC_Init();
 
	MotionDI_Initialize(&freq);
							
			/* Optional: Get version */
			 //MotionDI_GetLibVersion(lib_version);
			
			/* Optional: Modify knobs settings & set the knobs */
			
			MotionDI_getKnobs(&iKnobs);
			iKnobs.AccKnob.CalType = MDI_CAL_ONETIME;
			iKnobs.GyrKnob.CalType = MDI_CAL_ONETIME;
 
			BSP_SENSOR_ACC_GetOrientation(iKnobs.AccOrientation);
			BSP_SENSOR_GYR_GetOrientation(iKnobs.GyroOrientation);
 
			iKnobs.SFKnob.output_type = MDI_ENGINE_OUTPUT_NED;
			iKnobs.SFKnob.modx = DECIMATION;
			MotionDI_setKnobs(&iKnobs);
			
			AccCalMode = iKnobs.AccKnob.CalType;
			GyrCalMode = iKnobs.GyrKnob.CalType;
					
 
 if(LoggingInterface == USB_Datalog)
 {
 /* Initialize LED */
 BSP_LED_Init(LED1);
 BSP_LED_Off(LED1);
 }
 
 /* enable USB power on Pwrctrl CR2 register */
 HAL_PWREx_EnableVddUSB();
 HAL_PWREx_EnableVddIO2();
 
 if(LoggingInterface == USB_Datalog) /* Configure the USB */
 {
 /*** USB CDC Configuration ***/
 /* Init Device Library */
 USBD_Init(&USBD_Device, &VCP_Desc, 0);
 /* Add Supported Class */
 USBD_RegisterClass(&USBD_Device, USBD_CDC_CLASS);
 /* Add Interface callbacks for AUDIO and CDC Class */
 USBD_CDC_RegisterInterface(&USBD_Device, &USBD_CDC_fops);
 /* Start Device Process */
 USBD_Start(&USBD_Device);
 }
 else /* Configure the SDCard */
 {
 DATALOG_SD_Init();
 }
 
 /* Thread 1 definition */
 osThreadDef(THREAD_1, GetData_Thread, osPriorityAboveNormal, 0, configMINIMAL_STACK_SIZE*4);
 
 /* Thread 2 definition */
 osThreadDef(THREAD_2, WriteData_Thread, osPriorityAboveNormal, 0, configMINIMAL_STACK_SIZE*4);
 
 /* Start thread 1 */
 GetDataThreadId = osThreadCreate(osThread(THREAD_1), NULL);
 
 /* Start thread 2 */
	
 WriteDataThreadId = osThreadCreate(osThread(THREAD_2), NULL); 
 
 /* Start scheduler */
 osKernelStart();
 
 /* We should never get here as control is now taken by the scheduler */
 for (;;);
 
}
static void WriteData_Thread(void const *argument)
{
 
	
 (void) argument;
 osEvent evt;
 T_SensorsData *rptr;
 int size;
 char data_s[256];
	
 for (;;)
 {
		char entry[6];
				size=sprintf(entry, "for\n");
				osPoolFree(sensorPool_id, rptr); // free memory allocated for message
				CDC_Fill_Buffer(( uint8_t * )entry, size);
		
 evt = osMessageGet(dataQueue_id, osWaitForever); // wait for message
 if (evt.status == osEventMessage)
 {
			char entry[6];
				size=sprintf(entry, "if\n");
				osPoolFree(sensorPool_id, rptr); // free memory allocated for message
				CDC_Fill_Buffer(( uint8_t * )entry, size);
			
 if(evt.value.v == DATALOG_CMD_STARTSTOP)
 {
 if (SD_Log_Enabled) 
 {
 DATALOG_SD_Log_Disable();
 SD_Log_Enabled=0;
 }
 else
 {
 while(SD_Log_Enabled != 1)
 {
 if(DATALOG_SD_Log_Enable())
 {
 SD_Log_Enabled=1;
 osDelay(100);
 dataTimerStart();
 }
 else
 {
 //DATALOG_SD_Log_Disable();
 DATALOG_SD_DeInit();
 DATALOG_SD_Init();
 osDelay(100);
 }
 }
 }
 }
 else
 {
				char entry[6];
				size=sprintf(entry, "Entry\n");
				osPoolFree(sensorPool_id, rptr); // free memory allocated for message
				CDC_Fill_Buffer(( uint8_t * )entry, size);
				
 rptr = evt.value.p;
 
 if(LoggingInterface == USB_Datalog)
 {
										/* Dynamic Inclinometer API initialization function */
 		
					
					/*** Using Dynamic Inclinometer algorithm ***/
					//Timer_OR_DataRate_Interrupt_Handler()
					//{
					MDI_input_t data_in;
					MDI_output_t data_out;
					/* Get acceleration X/Y/Z in g */
					data_in.Acc[0] = rptr->acc.x; 
					data_in.Acc[1] = rptr->acc.y;
					data_in.Acc[2] = rptr->acc.z;
					
					/* Get angular rate X/Y/Z in dps */
					data_in.Gyro[0] = rptr->gyro.x;
					data_in.Gyro[1] = rptr->gyro.y;
					data_in.Gyro[2] = rptr->gyro.z;
					
					data_in.Timestamp = rptr->ms_counter;
					//data_in.Timestamp = HAL_GetTick() * 1000;
					/* Run Dynamic Inclinometer algorithm */
					
//					char msgg[25];
//					size=sprintf(msgg, lib_version);
//					osPoolFree(sensorPool_id, rptr); // free memory allocated for message
// CDC_Fill_Buffer(( uint8_t * )msgg, size);
 
					char hi[4];
					size=sprintf(hi, "Hi\n");
					osPoolFree(sensorPool_id, rptr); // free memory allocated for message
 CDC_Fill_Buffer(( uint8_t * )hi, size);
					
//					 size = sprintf(data_s, "TimeStamp: %ld\r\n Acc_X: %d, Acc_Y: %d, Acc_Z :%d\r\n Gyro_X:%d, Gyro_Y:%d, Gyro_Z:%d\r\n",
// rptr->ms_counter,
// (int)data_in.Acc[0], (int)data_in.Acc[1], (int)data_in.Acc[2],
// (int)data_in.Gyro[0], (int)data_in.Gyro[1], (int)data_in.Gyro[2]);
//											 osPoolFree(sensorPool_id, rptr); // free memory allocated for message
// CDC_Fill_Buffer(( uint8_t * )data_s, size);
 
//					
					
					MotionDI_update(&data_out, &data_in);
					char bye[4];
					size=sprintf(bye, "Bye\n");
					osPoolFree(sensorPool_id, rptr); // free memory allocated for message
 CDC_Fill_Buffer(( uint8_t * )bye, size);
					 
					/* Use data_out – output data from Dynamic Inclinometer algorithm */
					//}
																	 
				size = sprintf(data_s, "TimeStamp: %ld\r\n x-Rotation: %d, y-Rotation: %d, z-Rotation: %d\r\n x_accel: %d, y_accel: %d, z_accel: %d\r\n",
 data_in.Timestamp, (int)data_out.rotation[0], (int)data_out.rotation[1], (int)data_out.rotation[2], 
								(int)data_out.linear_acceleration[0], (int)data_out.linear_acceleration[1], (int)data_out.linear_acceleration[2]);
											 
 osPoolFree(sensorPool_id, rptr); // free memory allocated for message
 BSP_LED_Toggle(LED1);
 CDC_Fill_Buffer(( uint8_t * )data_s, size);
 }
 else
 {
 size = sprintf(data_s, "%ld, %d, %d, %d, %d, %d, %d, %d, %d, %d, %5.2f, %5.2f, %4.1f\r\n",
				 rptr->ms_counter,
				 (int)rptr->acc.x, (int)rptr->acc.y, (int)rptr->acc.z,
				 (int)rptr->gyro.x, (int)rptr->gyro.y, (int)rptr->gyro.z,
				 (int)rptr->mag.x, (int)rptr->mag.y, (int)rptr->mag.z,
				 rptr->pressure, rptr->temperature, rptr->humidity);
 osPoolFree(sensorPool_id, rptr); // free memory allocated for message
 DATALOG_SD_writeBuf(data_s, size);
 }
 }
 }
 }
}

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    February 23, 2022

    Hi @QAbba.1​ ,

    I see you posted a similar question here (LINK).

    The subject looks the same.

    Let's wait then for Miroslav support there.

    -Eleon