Skip to main content
IBo.1
Associate
December 30, 2020
Question

I have an L475 Discovery IoT node, I want to collect sensor data from the board and save it in a text file in my laptop which is USB connected to the board. I have tried Fprint and fwrite but it doesn't seem to work.

fp=fopen("Issamos.csv","w+");
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
	temp_value = BSP_TSENSOR_ReadTemp();
	int tmpInt1 = temp_value;
	float tmpFrac = temp_value - tmpInt1;
	int tmpInt2 = trunc(tmpFrac * 100000);
	snprintf(str_tmp,100," TEMPERATURE = %d.%02d\n\r", tmpInt1, tmpInt2);
 
	HAL_UART_Transmit(&huart1,( uint8_t * )str_tmp,sizeof(str_tmp),1000);
	fwrite(str_tmp, 100, 1,fp);
 
	 fclose(fp);
 

as you see I am collecting the data and using snprintf to display it in true studio, but writing it to a file doesn't work

This topic has been closed for replies.

3 replies

KnarfB
Super User
December 30, 2020

You cannot open a file on the host easily. But, you can transfer data via the serial connection included in the ST-LINK which is huart1

on the board. In order to do so, you implement a function _write in main.c:

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
int _write(int file, char *ptr, int len)
{
	HAL_UART_Transmit(&huart1, ptr, len, HAL_MAX_DELAY );
	return len;
}
/* USER CODE END 0 */

This function will be used by printf (instead of the "weak" do-nothing implementaion of _write in syscalls.c). From now on, you may use printf as you wish and the outputis transferred to the host. It can be read in a terminal program like TeraTerm or others by opening the ST-LINK serial port.

See STMs "STM32 microcontroller debug toolbox" document for more details.

In theory, it might be possible to implement other file related functions from syscalls.c too (like _open) with some protocols and stubs on the other side ("semihosting"). Don't know of a readily available solution though.

IBo.1
IBo.1Author
Associate
December 30, 2020

Dear Knarf,

Many thanks for the answer, I am not from an embedded system background and I am just starting.

As I said before, I am currently sending the data from the board to turbostudio terminal and I can see the data which seems correct.

I now, want to find a way to either save the data while streaming on mu pc, or copy it from the terminal to a file and then I would do some processing on it.

Could you please tell me how the function you gave me could help

Regards

TDK
December 30, 2020

Most terminal programs (PuTTY, RealTerm, Termite, others) have a mode which logs the console output directly to a file. I would look into a feature similar to that.

"If you feel a post has answered your question, please click ""Accept as Solution""."