Skip to main content
ABane.1
Associate II
February 17, 2023
Question

I have a STWINKT1B board with me. I am using Preditctive_Maintenence_BLE project of STM32CubeFunctionPack_PREDMNT1_V2.4.0. How to use IIS3DWB in this project?

..

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    ST Technical Moderator
    April 12, 2023

    Hi @ABane.1​ ,

    Preditctive_Maintenence_BLE has been done for ISM330DHCX, so to use it for IIS3DWB you need to include the sensor's drivers in the project (find it in \STM32CubeFunctionPack_PREDMNT1_V2.4.1\Drivers\BSP\Components\iis3dwb).

    However you should also modify Preditctive Maintenence parameters according to the new sensor, but this is a pretty tricky procedure but if you're in for a challenge this is a good opportunity to test yourself!

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.