Question
I have a question about the temperature compensation of the LPS22HH.
This is the result of getting the pressure value and temperature of LPS22HH.
①1051.5 hPa, 22.5 ℃
②1083. 8hPa, 30.7 ℃
This is the result of obtaining the pressure value of the pressure sensor 2SMPB-02B for comparison.
①1015.3 hPa
②1015.2 hPa
① is the value at a room temperature of 22°C.
② is the value about 30 seconds after heating with a dryer.
I am using STEVAL-MKI192V1.
There is a difference in pressure change due to temperature.
Am I missing some necessary setting?