Skip to main content
MJurk.1
Associate
Mar 30, 2020 1:11 PM UTC
Solved

I got the MLC working on the lsm6dsox. But when i enable stepcount on FIFO my MLC stops working ? these are the 3 lines , is there anyway i can use MLC and stepcount? or will i have to make my own step count tree?

/* Start Machine Learning Core configuration */

    for (uint32_t i = 0; i 

                              sizeof(ucf_line_t));

         i++)

    {

        lsm6dsox_write_reg(p_lsm6dsox, lsm6dsox_MLC[i].address,

                           (uint8_t *)&lsm6dsox_MLC[i].data, 1);

    }

    /*    Disable I3C interface   */

    lsm6dsox_i3c_disable_set(p_lsm6dsox, LSM6DSOX_I3C_DISABLE);

    /* Turn off Sensors */

    lsm6dsox_xl_data_rate_set(p_lsm6dsox, LSM6DSOX_XL_ODR_OFF);

    lsm6dsox_gy_data_rate_set(p_lsm6dsox, LSM6DSOX_GY_ODR_OFF);

    /*  Enable Block Data Update       */

    lsm6dsox_block_data_update_set(p_lsm6dsox, PROPERTY_ENABLE);

    //     /*

    //    * Set full scale

    //    */

    lsm6dsox_xl_full_scale_set(p_lsm6dsox, LSM6DSOX_4g);

    lsm6dsox_gy_full_scale_set(p_lsm6dsox, LSM6DSOX_2000dps);

    /*

   * Set FIFO watermark (number of unread sensor data TAG + 6 bytes

   * stored in FIFO) to 10 samples

   */

    lsm6dsox_fifo_watermark_set(p_lsm6dsox, 10);

    /*

       * Set FIFO batch XL/Gyro ODR to 12.5Hz

       */

    lsm6dsox_fifo_xl_batch_set(p_lsm6dsox, LSM6DSOX_XL_BATCHED_AT_26Hz);

    lsm6dsox_fifo_gy_batch_set(p_lsm6dsox, LSM6DSOX_XL_BATCHED_AT_26Hz);

    /*

       * Set FIFO mode to Stream mode (aka Continuous Mode)

    

       */

    lsm6dsox_fifo_mode_set(p_lsm6dsox, LSM6DSOX_STREAM_MODE);

 lsm6dsox_pin_int1_route_t int1_route;

    lsm6dsox_pin_int1_route_get(p_lsm6dsox, &int1_route);

    int1_route.int1_ctrl.int1_fifo_th = PROPERTY_ENABLE;

    lsm6dsox_pin_int1_route_set(p_lsm6dsox, &int1_route);

    /* Route signals on interrupt pin 1 */

    lsm6dsox_pin_int2_route_t pin_int2_route;

    lsm6dsox_pin_int2_route_get(p_lsm6dsox, &pin_int2_route);

    pin_int2_route.mlc_int2.int2_mlc1 = PROPERTY_ENABLE;

    lsm6dsox_pin_int2_route_set(p_lsm6dsox, &pin_int2_route);

    /* Configure interrupt pin mode notification */

    // lsm6dsox_int_notification_set(p_lsm6dsox, LSM6DSOX_BASE_PULSED_EMB_LATCHED);

    /* Set Output Data Rate.

   * Selected data rate have to be equal or greater with respect

   * with MLC data rate.

   */

    lsm6dsox_xl_data_rate_set(p_lsm6dsox, LSM6DSOX_XL_ODR_26Hz);

    lsm6dsox_gy_data_rate_set(p_lsm6dsox, LSM6DSOX_GY_ODR_26Hz);

    lsm6dsox_****_sens_set(p_lsm6dsox, LSM6DSOX_****_BASE_MODE);

    lsm6dsox_fifo_****_batch_set(p_lsm6dsox, PROPERTY_ENABLE);

    lsm6dsox_steps_reset(p_lsm6dsox);

    This topic has been closed for replies.
    MJurk.1
    MJurk.1Best answer
    Associate
    Nov 23, 2021 3:57 PM UTC

    you need to reset the mlc after writting registers to run off mlc

    3 replies

    AMALK.1
    Visitor II
    Jul 11, 2020 12:07 PM UTC

    Hi,

    I am having the same problem as you hare having. Did you solve it?

    What i have done on my side, is loading the UCF file file,

    From what i saw the the UCF file is actually overriding some of the gyro/acc output filter and changing the full scale. I have no idea if this is why the embedded functions and other non-mlc functionalities are not working properly.

    I have not found clearly any indications in the code that could lead to this kind of limitations.

    If anyone have clues why this happen?

    Thank you

    MJurk.1
    MJurk.1AuthorBest answer
    Associate
    Nov 23, 2021 3:57 PM UTC

    you need to reset the mlc after writting registers to run off mlc

    Eleon BORLINI
    ST Employee
    Nov 26, 2021 10:33 AM UTC

    Hi @MJurk.1​ ,

    great you come back to the Community after such a long time!

    And glad you shared the solution to the issue.

    -Eleon