Skip to main content
YBend.1
Associate III
July 7, 2022
Solved

I am using the STEVAL-STWINK1B board to acquire gyroscope data and comparing it with the Racelogic IMU04, however the data that the STWINK1B IMU fetches is the in mdps(milli degree per second) and the data the racelogic IMU fetches is in degrees per

For performing the conversion do I just have to convert degrees to millidegrees?

Because this conversion does not output a perfectly comparable result.

Racelogic IMU datasheet: Overview (racelogic.co.uk)

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    July 8, 2022

    Hi @YBend.1​ ,

    Yes, the conversion from milli-dps to dps is just a x1000 factor (or vice-versa).

    To be sure you are acquiring the same thing, you should check the band of Racelogic IMU04 gyroscope and the output data rate. This because there might be signal / noise in a range of frequencies not covered by one of the two sensors.

    -Eleon

    3 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    July 8, 2022

    Hi @YBend.1​ ,

    Yes, the conversion from milli-dps to dps is just a x1000 factor (or vice-versa).

    To be sure you are acquiring the same thing, you should check the band of Racelogic IMU04 gyroscope and the output data rate. This because there might be signal / noise in a range of frequencies not covered by one of the two sensors.

    -Eleon

    YBend.1
    YBend.1Author
    Associate III
    July 11, 2022

    Thanks @Eleon BORLINI​ 

    The Raceleogic IMU has a sampling rate of 20Hz while the ISM330DHCX sensor on the STWINKB1 board has a sampling rate of 6667Hz. I downsampled the data to compare the two to 20Hz.

    Can you please tell me how can I validate the signal / noise phenomenon that you have stated in the latter part of your answer.

    Thank you very much!!

    Eleon BORLINI
    ST Employee
    July 18, 2022

    Hi @YBend.1​ ,

    ok, they run at very different speeds.

    You can check if they are comparable at a noise / sensitivity level by acquiring the ISM330DHCX stream and then applying a filter at 20Hz in post processing.

    -Eleon