Skip to main content
AKuru.1
Associate
January 28, 2020
Question

I am about to develop my own firmware for STEVAL-MKI109V3 (with STEVAL-MKI159V1, which has the LSM9DS1). Could someone share source code a complete IOC file or even a complete demo app? If ST already sharing these, where do I find them? Thanks.

I am already able to build firmware, which blinks LEDs, but I would like to cut some corners.

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    January 28, 2020

    Hi @AKuru.1​ , you can find STEVAL-MKI109V3 .ioc file here.

    If you just want to interface LSM9DS1 and STEVAL-MKI109V3 in a custom way, it is not difficult to start a new project on STEVAL-MKI109V3 from scratch: you can base on STM32CubeIDE and create a project for STM32F401VE MCU and enabling the appropriate interfaces as described by the STEVAL-MKI109V3 schematic.

    If you want to control the Unico GUI, I suggest you to download the Unico lite source code, which enables you to modify part of the interface.

    Regards

    AKuru.1
    AKuru.1Author
    Associate
    January 28, 2020