Skip to main content
JMerc
Associate
September 4, 2019
Question

HTS221 Temperature sensor

Hello,

I have one Arduino MKR ENV board which has this sensor. The problem is that I'm reading higher temperature values than expected.

The routines that I use are :

For calibration:

 /**
 
 * HTS221_readCalibration
 
 *
 
 * Reads calibration values
 
 * @return char - != 0 if any error happened
 
 */
 
char HTS221::readCalibration(void) {
 
	unsigned char T0_degC_x8_H;
 
	unsigned char T0_degC_x8_L;
 
	unsigned char T1_degC_x8_H;
 
	unsigned char T1_degC_x8_L;
 
	
 
	unsigned char H0_rh_x2;
 
	unsigned char H1_rh_x2;
 
	
 
	int temp;
 
 
 
	DEBUG("HTS221 - Reading Calibration: ");
 
	DEBUG("\n\r");
 
	
 
	/**
 
 * Humidity calibration values
 
 */
 
	if((temp = readReg(HTS221_H0_RH_X2)) < 0) return 1;
 
	H0_rh_x2 = (unsigned char)temp;
 
	H0_rh = H0_rh_x2 / 2.0;
 
	
 
	DEBUG("HTS221 - H0_rh: ");
 
	DEBUGF(H0_rh, 2);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_H1_RH_X2)) < 0) return 2;
 
	H1_rh_x2 = (unsigned char)temp;
 
	H1_rh = H1_rh_x2 / 2.0;
 
	
 
	DEBUG("HTS221 - H1_rh: ");
 
	DEBUGF(H1_rh, 2);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_H0_T0_OUT_L)) < 0) return 3;
 
	H0_T0_out = (unsigned char)temp;
 
	if((temp = readReg(HTS221_H0_T0_OUT_H)) < 0) return 4;
 
	H0_T0_out |= ((unsigned char)temp << 8);
 
	
 
	DEBUG("HTS221 - H0_T0_out: ");
 
	DEBUGF(H0_T0_out, DEC);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_H1_T0_OUT_L)) < 0) return 5;
 
	H1_T0_out = (unsigned char)temp;
 
	if((temp = readReg(HTS221_H1_T0_OUT_H)) < 0) return 6;
 
	H1_T0_out |= ((unsigned char)temp << 8);
 
	
 
	DEBUG("HTS221 - H1_T0_out: ");
 
	DEBUGF(H1_T0_out, DEC);
 
	DEBUG("\n\r");
 
	
 
	
 
	/**
 
 * Temperature calibration values
 
 */
 
	if((temp = readReg(HTS221_T1T0_MSB)) < 0) return 7;
 
	DEBUG("HTS221_T1T0_MSB - 0x35: 0x");
 
	DEBUGF(temp, HEX); DEBUG(" decimal="); DEBUGF(temp, DEC);
 
	DEBUG("\n\r");
 
	T0_degC_x8_H = (unsigned char)(temp & 0x03);
 
	
 
	
 
	if((temp = readReg(HTS221_T0_DEGC_X8)) < 0) return 8;
 
	T0_degC_x8_L = (unsigned char)temp;
 
	DEBUG("HTS221_T0_DEGC_X8 - 0x32: 0x");
 
	DEBUGF(T0_degC_x8_L, HEX); DEBUG(" decimal="); DEBUGF(T0_degC_x8_L, DEC);
 
	DEBUG("\n\r");
 
	
 
	
 
	T0_degC = (((T0_degC_x8_H << 8) | T0_degC_x8_L)) / 8.0;
 
	DEBUG("HTS221 - T0_degC: ");
 
	DEBUGF(T0_degC, 2);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_T1T0_MSB)) < 0) return 9;
 
	T1_degC_x8_H = (unsigned char)((temp & 0x0C) >> 2);
 
	
 
	if((temp = readReg(HTS221_T1_DEGC_X8)) < 0) return 10;
 
	T1_degC_x8_L = (unsigned char)temp;
 
	DEBUG("HTS221_T1_DEGC_X8 - 0x33: 0x");
 
	DEBUGF(T1_degC_x8_L, HEX); DEBUG(" decimal="); DEBUGF(T1_degC_x8_L, DEC);
 
	DEBUG("\n\r");
 
	
 
	T1_degC = ((T1_degC_x8_H << 8) | T1_degC_x8_L) / 8.0;
 
	DEBUG("HTS221 - T1_degC: ");
 
	DEBUGF(T1_degC, 2);
 
	DEBUG("\n\r");
 
	
 
	
 
	if((temp = readReg(HTS221_T0_OUT_L)) < 0) return 11;
 
	T0_out = (unsigned char)temp;
 
	DEBUG("HTS221_T0_OUT_L - 0x3C: 0x");
 
	DEBUGF(T0_out, HEX); DEBUG(" decimal="); DEBUGF(T0_out, DEC);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_T0_OUT_H)) < 0) return 12;
 
	DEBUG("HTS221_T0_OUT_H - 0x3D: 0x");
 
	DEBUGF(temp, HEX); DEBUG(" decimal="); DEBUGF(temp, DEC);
 
	DEBUG("\n\r");
 
	
 
	T0_out |= ((unsigned char)temp << 8);
 
	DEBUG("HTS221 - T0_out: ");
 
	DEBUGF(T0_out, DEC);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_T1_OUT_L)) < 0) return 13;
 
	T1_out = (unsigned char)temp;
 
	DEBUG("HTS221_T1_OUT_L - 0x3E: 0x");
 
	DEBUGF(T1_out, HEX); DEBUG(" decimal="); DEBUGF(T1_out, DEC);
 
	DEBUG("\n\r");
 
	
 
	if((temp = readReg(HTS221_T1_OUT_H)) < 0) return 14;
 
	DEBUG("HTS221_T1_OUT_H - 0x3F: 0x");
 
	DEBUGF(temp, HEX); DEBUG(" decimal="); DEBUGF(temp, DEC);
 
	DEBUG("\n\r");
 
	
 
	T1_out |= ((unsigned char)temp << 8);
 
	DEBUG("HTS221 - T1_out: ");
 
	DEBUGF(T1_out, DEC);
 
	DEBUG("\n\r");
 
	
 
	return 0;
 
}

For reading the values

float HTS221::readTemperature(void) {
 
	unsigned char temp;
 
	int value;
 
	float result;
 
	
 
	value = readReg(HTS221_TEMP_OUT_H);
 
	temp = (unsigned char)readReg(HTS221_TEMP_OUT_L);
 
	value = (value << 8) | temp;
 
	
 
	DEBUG("HTS221 - T_OUT: ");
 
	DEBUGF(value, DEC);
 
	DEBUG("\n\r");
 
	
 
	result = (((float)value - T0_out)/(T1_out - T0_out)) * (T1_degC - T0_degC) + T0_degC;
 
	
 
	DEBUG("HTS221 - Temperature value readed: ");
 
	DEBUGF(result, 2);
 
	DEBUG("\n\r");
 
	
 
	return result;
 
}

The registers' values are:

HTS221_T1T0_MSB - 0x35: 0xC4 decimal=196

HTS221_T0_DEGC_X8 - 0x32: 0xA7 decimal=167

HTS221 - T0_degC: 20.87

HTS221_T1_DEGC_X8 - 0x33: 0x14 decimal=20

HTS221 - T1_degC: 34.50

HTS221_T0_OUT_L - 0x3C: 0x3 decimal=3

HTS221_T0_OUT_H - 0x3D: 0x0 decimal=0

HTS221 - T0_out: 3

HTS221_T1_OUT_L - 0x3E: 0xEB decimal=235

HTS221_T1_OUT_H - 0x3F: 0x2 decimal=2

HTS221 - T1_out: 747

HTS221 - T_OUT: 354

HTS221 - Temperature value readed: 27.30

Is it problem of a faulty device?

Thanks in advance

Jordi Mercader

    This topic has been closed for replies.

    7 replies

    Eleon BORLINI
    ST Employee
    September 26, 2019

    Hi @JMerc​ , sorry for the late answer, but it could be a lot-related issue... Basically your issue is that you are reading a temperature value constantly over a certain value, or does the value oscillate between a correct t range and higher temperatures? Do you have the possibility to test another device? Regards

    JMerc
    JMercAuthor
    Associate
    September 30, 2019

    Hi Eleon,

    Thanks for your answer.

    The reading is always around 3ºC to 5ºC above the real temperature.

    I have another MKR ENV board and the readings were similar.

    Can you check if the calibration parameters are faulty?

    Best regards

    Jordi Mercader

    Eleon BORLINI
    ST Employee
    September 30, 2019

    ​Hi Jordi, please check this thread if can be of your help. No issues about humidity value? Can you share the regmap dup described at that link? Regards