Skip to main content
AFeil.1445
Visitor II
June 2, 2020
Question

HTS221 Temperature measuring

Hi,

we are using HTS221TR. In the datasheet it is not clear what is the temperature range what the sensor can measure -40...85? +15°C....40?

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    June 3, 2020

    Hi @AFeil.1445​ , the HTS221 can detect the temperature in the entire -40°C...+120°C range, but with different accuracies centered around 25°C, which is the calibration point:

    • typ +-0.5 between 15°C and 40°C
    • typ +-1 from 0°C to 15°C and from 40°C to 60°C
    • typ +-2 from -40°C to 0°C and from 60°C to 120°C

    (p.8 of the datasheet)

    0693W000001pupRQAQ.png

    Regards