Skip to main content
Remco Kleine
Associate II
Mar 27, 2018 7:03 AM UTC
Question

HTS221 Cal. Coeficients

Posted on March 27, 2018 at 09:03

Hello,

I implemented the software for the HTS221 in my project and all is working. 

But what I find strange is this, some calibration coefficients are negative!

H0_T0_OUT is -2

H1_T0_OUT = -11728

Although they are negative, the reading for temperature is OK  (seems to be < 1 degrees lower than my reference )

But the Humidity reading is 10% off ( too low)

Now in the examples from the datasheet, the coefficients were positive. 

For example my reading of H_T_OUT = - 784. and in the datasheet it is 5000

Why are these coeficients in the s16 format? Can they be really negative? They are like raw ADC value's right?

Regards Remco

    This topic has been closed for replies.

    2 replies

    ST Employee
    Mar 29, 2018 1:28 PM UTC
    Posted on March 29, 2018 at 15:28

    Yes, the coefficients can be negative.

    What is you reference humidity sensor? 

    Remco Kleine
    Associate II
    Apr 4, 2018 10:29 AM UTC
    Posted on April 04, 2018 at 12:29

    My Reference is an Extech RH101 meter.  I have 3 HTS sensors and they are all  10 to15% lower than this reference.