Skip to main content
ark2
Associate II
November 1, 2022
Question

How to write multiple sensor modules with stm32 spi

I don't know how to use several sensor modules with stm32 spi

They told me to use the code I received, but I think it's wrong because even if I connect the sensor and run the code, the same value comes out

Do I have to fix all the codes below? Or do I just have to change it a little bit?

 Please tell me how I can use multiple sensor modules with one spi

// spi -speed = 2 "=" 64.5MBits => 0x00
 // spi -speed = 4 "=" 32.25MBits => 0xFF
 // spi -speed = 8 "=" 16.125MBits => 
 // spi -speed = 16 "=" 8.0825MBits => 0xFF
 // spi -speed = 256 "=" 503.906MBits => 
 uint8_t T_buffer1[] = {0xC0, 0x00 };
 uint8_t T_buffer2[] = {0x05, 0x00 };
 uint8_t T_buffer3[] = {0x07, 0x03 };
 uint8_t T_buffer4[] = {0x0B, 0x00};
 uint8_t T_buffer6[] = {0x0D, 0x00};
 uint8_t T_buffer7[] = {0x0F, 0x00};
 uint8_t T_buffer8[] = {0x11, 0x00};
 uint8_t T_buffer9[] = {0x13, 0x00};
 uint8_t T_buffer10[] = {0x15, 0x00};
 uint8_t T_buffer11[] = {0x17, 0x00};
 uint8_t T_buffer12[] = {0x19, 0x00};
 uint8_t T_buffer13[] = {0x00};
 uint8_t T_buffer_Cmd[] = {0xA0, 0x00,0xFF,0xFF};
 uint8_t T_buffer_Capture0[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture1[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture2[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture3[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture4[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture5[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture6[] = {0x00, 0x00,0xFF,0xFF,128};
 uint8_t T_buffer_Capture7[] = {0x00, 0x00,0xFF,0xFF,128};
 
 // --> ch0
 // uint8_t T_buffer_C1[] = {0x03,0x01};
 // uint8_t T_buffer_C2[] = {0x05,0xFE}; 
 // uint8_t T_buffer_C3[] = {0x0B,0x06}; //0B : 0,0D : 1 
 // --> ch1
 // uint8_t T_buffer_C1[] = {0x03,0x02};
 // uint8_t T_buffer_C2[] = {0x05,0xFD}; 
 // uint8_t T_buffer_C3[] = {0x0D,0x06}; //0B : 0,0D : 1 
 
 uint8_t T_buffer_C1[] = {0x03,0x01,0x00}; // 80: 7
 uint8_t T_buffer_C2[] = {0x05,0xFE,0x00}; //7F: 7 
 uint8_t T_buffer_C3[] = {0x0B,0x06,0x00}; //0B : 0,0D : 1 19: 7
 uint8_t T_buffer_C33[] = {0xA0,0x00,0x00,0x00};
 uint8_t T_buffer_C4_3[] = {0x00,0x00,0x00,0x00};
 uint8_t T_buffer_C5[] = {0xFF,0xFF,0x00,0x00};
 
 uint8_t T_buffer_C1_[] = {0x85,0x00}; // 80: 7
 uint8_t T_buffer_C2_0[] = {0x0B,0x00}; //7F: 7 
 uint8_t T_buffer_C2_1[] = {0x0D,0x05}; //7F: 7 
 uint8_t T_buffer_C2_2[] = {0x0F,0x05}; //7F: 7 
 uint8_t T_buffer_C2_3[] = {0x11,0x05}; //7F: 7 
 uint8_t T_buffer_C2_4[] = {0x13,0x05}; //7F: 7 
 uint8_t T_buffer_C2_51[] = {0x15,0x05}; //7F: 7 
 uint8_t T_buffer_C2_6[] = {0x17,0x05}; //7F: 7 
 uint8_t T_buffer_C2_7[] = {0x19,0x0F}; //7F: 7 
 uint8_t T_buffer_C33_[] = {0xA0,0x00,0xFF,0xFF};
 uint8_t T_buffer_C4_[] = {0xFF,0xFF,0xFF,0xFF};
 uint8_t T_buffer_C5_[] = {0x00,0x00,0x00,0x00}; 
 
 
 uint8_t T_buffer_C1_5[] = {0x03,0x80};
 uint8_t T_buffer_C2_5[] = {0x05,0x7F}; 
 uint8_t T_buffer_C3_5[] = {0x19,0x06}; //0B : 0,0D : 1 
 uint8_t T_buffer_C33_5[] = {0xA0,0x00};
 uint8_t T_buffer_C4_5[] = {0xFF,0xFF};
 uint8_t T_buffer_C5_5[] = {0xC0,0x00,0xFF,0xFF};
 
 HAL_SPI_Transmit(&hspi2, T_buffer_C1_, 2, 5);
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_0, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); /*
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_1, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_2, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_3, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_4, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_51, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_6, 2, 5); 
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); */ 
 HAL_SPI_Transmit(&hspi2, T_buffer_C2_7, 2, 5);
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C5_5, 2, 5);
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi2, T_buffer_C5_5+2, 2, 5);
HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5); 
 
 HAL_SPI_Transmit(&hspi5, T_buffer_C1_, 2, 5);
HAL_SPI_Receive(&hspi5,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi5, T_buffer_C2_0, 2, 5); 
HAL_SPI_Receive(&hspi5,R_buffer_Spi2, 2, 5); 
 HAL_SPI_Transmit(&hspi5, T_buffer_C2_7, 2, 5);
HAL_SPI_Receive(&hspi5,R_buffer_Spi5, 2, 5); 
 HAL_SPI_Transmit(&hspi5, T_buffer_C5_5, 2, 5);
HAL_SPI_Receive(&hspi5,R_buffer_Spi5, 2, 5); 
 HAL_SPI_Transmit(&hspi5, T_buffer_C5_5+2, 2, 5);
HAL_SPI_Receive(&hspi5,R_buffer_Spi5, 2, 5); 
 
 for(;;)
 { 
 osDelay(1);
 if(timer_state==1)
 { 
 for(int i=0; i<8; i++)
 {
 T_buffer_C5_5[0] = 0xC0 + (4 * i);
 
 HAL_Delay(1);
 HAL_SPI_Transmit(&hspi2, T_buffer_C5_, 2, 5);
 HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5);
 HAL_SPI_Transmit(&hspi2, T_buffer_C4_, 2, 5);
 HAL_SPI_Receive(&hspi2,R_buffer_Spi2, 2, 5);
 
 Temp_Ch0 = R_buffer_Spi2[3];
 Temp_Ch0 = Temp_Ch0 << 8;
 Temp_Ch0 += R_buffer_Spi2[2];
 
 R_buffer_Spi2_Temp[0] = R_buffer_Spi2[3];
 R_buffer_Spi2_Temp[1] = R_buffer_Spi2[2];
 R_buffer_Spi2_Temp[2] = 0x0D;
 R_buffer_Spi2_Temp[3] = 0x0A; 
 
 HAL_Delay(5);
 
 if(i==0)
 {
 Temp_Ch0 = 0;
 Temp_Ch0 = R_buffer_Spi2_Temp[1];
 Temp_Ch0 = Temp_Ch0 << 8;
 Temp_Ch0 += R_buffer_Spi2_Temp[0];
 set_sensordata(&Temp_Ch0, 0);
 }
 else if(i==7)
 {
 Co2_2_Ch7 = 0;
 Co2_2_Ch7 = R_buffer_Spi2_Temp[1];
 Co2_2_Ch7 = Co2_2_Ch7 << 8;
 Co2_2_Ch7 += R_buffer_Spi2_Temp[0];
 set_sensordata(&Co2_2_Ch7 , 8);
 }
 }
 
 
 T_buffer_C5_5[0]=0xC0;
 
 memset(R_buffer_Spi5, 0x00, sizeof(R_buffer_Spi5));
 memset(R_buffer_Spi2_Temp, 0x00, sizeof(R_buffer_Spi2_Temp));
 
 timer_state= 0;
 }
 }

This topic has been closed for replies.