Skip to main content
ATat.1
Visitor II
Jul 8, 2021 9:07 AM UTC
Solved

How to verify accelerometer data is correct or not?

I have read the accelerometer data using(H3LIS100DL) sensor then I got some negative value x=-3, y=-2, z=-1. I used these register OUT_X(29h), OUT_Y(2Bh), OUT_Z(2Dh). My question is how to verify these accelerometer X, Y, Z data is correct or not?

This topic has been closed for replies.
TBomb.1
TBomb.1Best answer
Visitor II
Jul 14, 2021 3:44 PM UTC

Hi, usually ST sensor shows 1g along z axis and close to 0g along the other axis.

Probably for the H3LIS100DL the zero g offset is higher (+-1.5g I see from the datasheet), since the full scale is high.

LSB and mg are of same order of magnitude and can be negative.

You can try hitting the device and see if the output on some axis change significantly.

https://www.st.com/resource/en/datasheet/h3lis100dl.pdf

Tom

1 reply

TBomb.1
TBomb.1Best answer
Visitor II
Jul 14, 2021 3:44 PM UTC

Hi, usually ST sensor shows 1g along z axis and close to 0g along the other axis.

Probably for the H3LIS100DL the zero g offset is higher (+-1.5g I see from the datasheet), since the full scale is high.

LSB and mg are of same order of magnitude and can be negative.

You can try hitting the device and see if the output on some axis change significantly.

https://www.st.com/resource/en/datasheet/h3lis100dl.pdf

Tom