Skip to main content
LCher.1
Visitor II
March 29, 2021
Question

How to use the PDM_FIlter function

  • March 29, 2021
  • 1 reply
  • 1385 views

Hi,

I created a small board with STM32F446MEY6TR and SPK0415HM4H-B MEMS microphone. I can read the data from the mic via I2S interface in a chinks of 100*16 samples. Now I want to filter the data with the PDM_FIlter function, but I'm not sure how to pass the arguments, as UM2372 is not very specific about this. Here is my main function:

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_CRC_Init();
 MX_PDM2PCM_Init();
 MX_I2S2_Init();
 /* USER CODE BEGIN 2 */
 
 uint16_t pdm_data[100];
 int16_t pcm_data[16];
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 // read the i2s data
	 HAL_StatusTypeDef result = HAL_I2S_Receive(&hi2s2, &pdm_data[0], 100, 100);
 
	 uint32_t error_code = PDM_Filter(pdm_data, pcm_data, &PDM1_filter_handler);
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

The PDM_FIlter function returns values from -8 to 8, which is too less.

Thank you!

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
March 30, 2021

Hi @LCher.1​ ,

even if you are using a non-ST microphone (it's from ), the PDM_filter function should work in the same way.

Can you please first check this other community thread, if it might be related to your issue?

-Eleon