Hi @JeongHoYong ,
To properly configure the LSM6DSL sensor, the following registers need to be set:
- CTRL8_XL (17h)
This register controls the high-pass path filter.
The bandwidth column depends on the value of HPCF_XL[1:0]:
- If HPCF_XL[1:0] = 00, the bandwidth relates to the slope filter.
- If HPCF_XL[1:0] = 01, 10, or 11, the bandwidth refers to the high-pass (HP) filter.
- CTRL1_XL (10h)
This register is used to set the Output Data Rate (ODR), Full Scale range, and the LPF1 (Low Pass Filter 1).
- Enabling the second LPF
If you want to add a second low-pass filter, you can enable it via the CTRL8_XL (17h) register.
To review the possible values and configurations, please refer to the official sensor page:
Specifically, in the datasheet, refer to:
- Chapters 9.13 and 9.20 for detailed register characteristics
- Section 5.4.2 for the sensor block diagram
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.