Skip to main content
LClad.1
Associate
March 13, 2020
Question

How to use INT1 or INT2 interrupts in lsm6dso with relative tilt function

Hi,

I'm trying to implement a relative tilt function using lsm6dso with nrf52832 processor.

Following the AN5192, the procedures to enable tilt detection are:

1.Write 80h to FUNC_CFG_ACCESS// Enable access to embedded functions registers

2.Write 10h to EMB_FUNC_EN_A// Enable tilt detection

3.Write 10h to EMB_FUNC_INT1// Tilt interrupt driven to INT1 pin

4.Write 80h to PAGE_RW// Enable latched mode for embedded functions

5.Write 00h to FUNC_CFG_ACCESS// Disable access to embedded functions registers

6.Write 02h to MD1_CFG// Enable embedded functions interrupt routing

7.Write 20h to CTRL1_XL// Turn on the accelerometer// ODR_XL = 26 Hz, FS_XL = ±2 g

Below is my code:

void LSM6DSO_CFG(){

   ret_code_t err_code;

   uint8_t dataToWrite = 0; //Temporary variable

   uint8_t func_cfg_access = 0x80U;

   err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, FUNC_CFG_ACCESS,&func_cfg_access, sizeof(func_cfg_access),true); // enable gyro and accel data ready interrupt on INT1

   APP_ERROR_CHECK(err_code);

   func_cfg_access = 0x10U; //tilt detection

   err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, EMB_FUNC_EN_A,&func_cfg_access, sizeof(func_cfg_access),true); // enable gyro and accel data ready interrupt on INT1

   APP_ERROR_CHECK(err_code);

   func_cfg_access = 0x10U; //tilt interrupt

   err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, EMB_FUNC_INT1,&func_cfg_access, sizeof(func_cfg_access),true); // enable gyro and accel data ready interrupt on INT1

   APP_ERROR_CHECK(err_code);

   func_cfg_access = 0x80U; //Enable latched mode

   err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, PAGE_RW,&func_cfg_access, sizeof(func_cfg_access),true); // enable gyro and accel data ready interrupt on INT1

   APP_ERROR_CHECK(err_code);

   func_cfg_access = 0x00U;

   err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, FUNC_CFG_ACCESS,&func_cfg_access, sizeof(func_cfg_access),true); // enable gyro and accel data ready interrupt on INT1

   APP_ERROR_CHECK(err_code);

   func_cfg_access = 0x02U;

   err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, MD1_CFG,&func_cfg_access, sizeof(func_cfg_access),true); // enable gyro and accel data ready interrupt on INT1

   APP_ERROR_CHECK(err_code);

   dataToWrite = 0x20U;

 err_code = write_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H, LSM6DSO_CTRL1_XL_REG,&dataToWrite, sizeof(dataToWrite),true);

 APP_ERROR_CHECK(err_code);

}

//===================================================

int main(void)

{

    APP_ERROR_CHECK(NRF_LOG_INIT(NULL));

   NRF_LOG_DEFAULT_BACKENDS_INIT();

    ret_code_t ret;

   twi_init();

    gpio_init(); //enable pin interrupt

   LSM6DSO_CFG();

   NRF_LOG_INFO("\r\nTWI sensor example started.");

   NRF_LOG_FLUSH();

   while (true)   {

     

        LSM6DSO_READ();

   }

}

//===================================================

void LSM6DSO_READ(void)

{

   ret_code_t err_code;

   uint8_t rx_data = EMB_FUNC_STATUS;

   err_code = read_LSM6DSO(m_twi_lsm6ds0, LSM6DSO_I2C_ADD_H,EMB_FUNC_STATUS ,&rx_data, sizeof(rx_data),true);

   APP_ERROR_CHECK(err_code);

}

I was enabled interrupt in nrf and tested independentlly with success, but using osciloscope, the pin int1 connected doesn't work.

Anyone can help me?

Laerte

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    March 20, 2020

    Hi @LClad.1​ , I don't understand if you was able to detect the interrupt or not... Did you check the INT1_TILT bit of the EMB_FUNC_INT1 (0Ah) register by polling it, to see if it is set to '1', even if not routed on the INT1 pin? Regards