Skip to main content
falconcrew42
Visitor II
December 9, 2019
Question

How to setup FIFO for LIS2HH12?

I am using LIS2HH12 with Atmel ATSAM4E8C and am able to read registers and write to registers.

When I read FIFO_SRC register (0x2F) I get Bit EMPTY=1 and in STATUS register (0x27) ZYXDA is constantly 0. I am following the example from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2hh12_STdC/example/read_data_simple.c and has tried to enable FIFO in CTRL3 register (0x22) and FIFO_CTRL register (0x2E), but still no data in FIFO.

Is there any setup steps I am missing?

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    December 11, 2019

    Hi @Philip Jönsson​ , unfortunately there are no LIS2HH12 example related to the FIFO directly available on Github repository. So I suggest you to take inspiration from the Lis3dh examples for the multi-read FIFO, because the control registers of the FIFO in the two cases are the same. I also suggest you to compare your code with p.34 and sgg of the AN4662. Regards

    void example_main_lis3dh_fifo(void)
    {
     /*
     * Initialize mems driver interface
     */
     stmdev_ctx_t dev_ctx;
     
     dev_ctx.write_reg = platform_write;
     dev_ctx.read_reg = platform_read;
     dev_ctx.handle = &hi2c1;
     
     /*
     * Initialize platform specific hardware
     */
     platform_init();
     
     /*
     * Check device ID
     */
     lis3dh_device_id_get(&dev_ctx, &whoamI);
     if (whoamI != LIS3DH_ID)
     {
     while(1)
     {
     /* manage here device not found */
     }
     }
     
     /*
     * Enable Block Data Update
     */
     lis3dh_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
     
     /*
     * Set Output Data Rate to 25 hz
     */
     lis3dh_data_rate_set(&dev_ctx, LIS3DH_ODR_25Hz);
     
     /*
     * Set full scale to 2 g
     */
     lis3dh_full_scale_set(&dev_ctx, LIS3DH_2g);
     
     /*
     * Set operating mode to high resolution
     */
     lis3dh_operating_mode_set(&dev_ctx, LIS3DH_HR_12bit);
     
     /*
     * Set FIFO watermark to 25 samples
     */
     lis3dh_fifo_watermark_set(&dev_ctx, 25);
     
     /*
     * Set FIFO mode to Stream mode: Accumulate samples and
     * override old data
     */
     lis3dh_fifo_mode_set(&dev_ctx, LIS3DH_DYNAMIC_STREAM_MODE);
     
     /*
     * Enable FIFO
     */
     lis3dh_fifo_set(&dev_ctx, PROPERTY_ENABLE);
     
     while(1)
     {
     uint8_t flags;
     uint8_t num = 0;
     
     /*
     * Check if FIFO level over threshold
     */
     lis3dh_fifo_fth_flag_get(&dev_ctx, &flags);
     if (flags)
     {
     /*
     * Read number of sample in FIFO
     */
     lis3dh_fifo_data_level_get(&dev_ctx, &num);
     while (num-- > 0)
     {
     /*
     * Read XL samples
     */
     lis3dh_acceleration_raw_get(&dev_ctx, data_raw_acceleration.u8bit);
     acceleration_mg[0] =
     lis3dh_from_fs2_hr_to_mg(data_raw_acceleration.i16bit[0]);
     acceleration_mg[1] =
     lis3dh_from_fs2_hr_to_mg(data_raw_acceleration.i16bit[1]);
     acceleration_mg[2] =
     lis3dh_from_fs2_hr_to_mg(data_raw_acceleration.i16bit[2]);
     
     sprintf((char*)tx_buffer, "Acceleration [mg]:%4.2f\t%4.2f\t%4.2f\r\n",
     acceleration_mg[0], acceleration_mg[1], acceleration_mg[2]);
     tx_com(tx_buffer, strlen((char const*)tx_buffer));
     }
     }
     }
    }