Skip to main content
WYang.9
Visitor II
February 15, 2023
Question

How to continuously read LSM6DSRTR data under Linux iio?

I am using​ LSM6DSRTR, and the device-tree compatible is "st,lsm6dsr".

I can see two iio device node under

​

/sys/bus/iio/devices/iio:device1
/sys/bus/iio/devices/iio:device2

But when I try to read in a python loop, it gets really slow.

​Anyway better to read it?

 def getData(self, path):
 fd = open(path, "r")
 data = fd.read().strip()
 fd.close()
 return data
 
 def testData(self):
 iio_oneshot_path = "/sys/bus/iio/devices/iio:device2/in_accel_x_raw"
 fd = open(iio_oneshot_path, "r")
 
 while self.refresh:
 self.accX = self.getData('/sys/bus/iio/devices/iio:device2/in_accel_x_raw')
 self.accY = self.getData('/sys/bus/iio/devices/iio:device2/in_accel_y_raw')
 self.accZ = self.getData('/sys/bus/iio/devices/iio:device2/in_accel_z_raw')
 self.gyroX = self.getData('/sys/bus/iio/devices/iio:device1/in_anglvel_x_raw')
 self.gyroY = self.getData('/sys/bus/iio/devices/iio:device1/in_anglvel_y_raw')
 self.gyroZ = self.getData('/sys/bus/iio/devices/iio:device1/in_anglvel_z_raw')
 print(self.accX)
 time.sleep(0.01)

​

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    ST Technical Moderator
    April 12, 2023

    Ciao @WYang.9​ ,

    Welcome to ST Community!

    The most recommended way to read data in continuous mode is to use the IIO buffer interface and for this I suggest the generic_buffer tool or the libiio test application iio_read.

    If it is necessary to read the data via raw data to speed up the reading procedure it's recommended to set a high ODR because when you use raw data read the driver turn on the device than expect an ODR and furthermore the first samples must be discarded because the device is turned on, this means waiting much longer than an ODR.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.