Skip to main content
Associate
May 10, 2026 7:45 PM UTC
Question

how to connect steval mk boxpro with ble mesh

I am currently working on a project using Steval mkboxpro and I would like to implement BLE Mesh communication between them. I am still learning and I was wondering if you could give me some guidance or recommend resources on how to do this 
Any help or advice would be greatly appreciated.

6 replies

Associate III
May 11, 2026 12:24 PM UTC

I having been working with the device over USB, I have strong doubts that the ST people will reply, I could be wrong, but I doubt it.  

Why would you want to do such a thing, the data is tremendous, about 5 days of data from a single device is 131 GB for useful analysis.  it is sitting on a separate hard drive. 

yocoAuthor
Associate
May 11, 2026 3:29 PM UTC

i have a project and this is mandatory 

Associate III
May 11, 2026 7:17 PM UTC

I do not use BLE if I can avoid it. Sorry

yocoAuthor
Associate
May 12, 2026 1:04 PM UTC

Merged with existing thread - please don't start multiple threads on the same topic.


i want to implement BLE Mesh communication between two sensorTile box pro so i flashed the fp sns blemesh1 on the card with stm32CubeProgrammer (on dfu mode) and then i used the app st ble mesh but i can't do the provisoning !!!!!

Associate III
May 12, 2026 1:30 PM UTC

I am sorry, but I only have one Pro at the moment, my others are in London and it is being used in a brick experiment.  

Do you get an error or nothing?  

 

Federica Bossi
ST Technical Moderator
Jun 15, 2026 8:20 AM UTC

Hi ​@yoco ,

Have you already looked at our user manual?

You can also use this one if you need something more detailed.

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.