Skip to main content
ersan
Associate III
August 30, 2012
Question

How to calculate LSB/dps Value? Did not find in Datasheet (LPR450AL gyro)

Posted on August 31, 2012 at 01:40

Hi,

in the example code of the LPR430AL there are written these values in the Header. one is from datasheet but where is the other from ? LSB/dps ? Where can i get my LSB value?

/*!<300dps Full Scale Pitch axis Sensitivity [ mV/dps ]see LPR430AL datasheet*/ #define Gyro_Sensitivity_P_300dps 3.33

/*!<300dps Full Scale Pitch axis Sensitivity [ LSB/dps ]*/

#define Gyro_SensitivityLSB_P_300dps 4.13

I need the LSB Value to calculate the Densivity for the LPR45AL.

Please Help

WR

Ersan

#lpr450al-gyro-lsb-value-stm32

    This topic has been closed for replies.

    1 reply

    harinath
    Associate III
    August 31, 2012
    Posted on August 31, 2012 at 04:33

    Hi Ersan,

    Gyro_Sensitivity_P_300dps  =     3.33

    STM32F103 microcontroller's 12-bit ADC is used to digitize Gyro signal.

    Gyro_SensitivityLSB_P_300dps   = (212 -1) / (300*3.3)

    Gyro_SensitivityLSB_P_300dps  =    4.13

    4.13 is the sensitivity of 4x amplified output.

    Now, sensitivity when not amplified is :

    Gyro_SensitivityLSB_R_1200dps = 4.13/4 = 1.0325Hari