Skip to main content
Associate II
May 26, 2025 9:07 AM UTC
Question

How to Achieve Accurate Acceleration and Velocity RMS Below 40 Hz with IIS3DWB?

I'm working with the IIS3DWB high-performance MEMS accelerometer and using it to calculate both acceleration RMS and velocity RMS values.

While the datasheet specifies a frequency response from DC to 6 kHz (±3 dB), I’ve noticed in practice that reliable and accurate RMS measurements only begin to appear from around 40 Hz onwards.

After enabling the digital high-pass filter (HPF) as shown in the documentation (see attached figure), I understand that the minimum cutoff is ODR/800, which translates to 33 Hz at an ODR of 26667 Hz. This explains the attenuation of low-frequency components and might be contributing to the inaccuracy in the 2–40 Hz band.

What is the best way to achieve accurate acceleration and velocity RMS values in the 2 Hz to 40 Hz frequency range using the IIS3DWB?

Any suggestions or community experience on low-frequency analysis with this sensor?

This topic has been closed for replies.

4 replies

Federica Bossi
ST Technical Moderator
May 29, 2025 9:15 AM UTC

Hi @Rishabh_Rathod ,

To measure within the frequency range of 2 to 40 Hz, we can suggest two different approaches. The common step for both solutions is:

  • Set the bit 3 of the CTRL8_XL register to 0, thereby setting the FDS bit to 0 (refer to section 9.17 of the Datasheet), and choose not to enable the high-pass filter (HPF).

The two possibilities involve whether or not to enable the low-pass filter (LPF):

  1. Solution 1:
    • Set LPF2_XL_EN to 0 (disable LPF), acquire data at the maximum output data rate (ODR), and then process the data to extract the necessary information. This approach will result in data redundancy.
  2. Solution 2:
    • Set LPF2_XL_EN to 1 (enable LPF) and choose a cutoff frequency based on the desired precision or the amount of data you wish to process for your measurement. For example, for the 2-40 Hz range, you might set HPCF_XL_[2:0] to 5.

We encourage you to try this configuration and let us know the results.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
May 30, 2025 11:47 AM UTC

Thank you for the helpful suggestions.

I tried disabling the HPF as recommended by setting CTRL8_XL.FDS = 0. However, I observed that doing so introduces a DC component in the acceleration signal, which artificially increases both acceleration RMS and velocity RMS values — especially noticeable in integrated velocity due to drift accumulation.

I’m working on a solution that aims to provide accurate RMS values over the full bandwidth from 10 Hz to 6.3 kHz, matching the sensor’s effective frequency response.

A few points and follow-up questions:

  • Is it possible to remove the DC component from the acceleration signal without using the built-in HPF?
    (e.g., using a software-based approach or offset correction method)

  • I’m basing my code on the MotionSP library. From my experience, the software HPF implementation there does reasonably well for acceleration RMS in the 10 Hz–6.3 kHz range.

  • However, when calculating velocity RMS (via integration), the SW HPF does not sufficiently eliminate low-frequency drift or if aggressively filtered remove low frequency signal components itself.

Would appreciate any recommendations for:

  • A robust software filtering technique that works well for integration (e.g., bandpass or detrending filters)

  • ST’s suggestions or best practices for achieving stable velocity RMS across the full sensor bandwidth, especially avoiding the DC bias when HPF is disabled.

  • Also for Motion SP what are the general values for parameters (smooth, Lambda, GAMMA)

Thanks again for the support!

Federica Bossi
ST Technical Moderator
Jun 6, 2025 3:00 PM UTC

Hi @Rishabh_Rathod ,

If you do not want to limit the band from 40Hz to 6.3KHz (and not from 10Hz) the only possible solution is to use an HPF sw and if it is not enough the only solution is to create an analog filter at least of 2-3 order ( with fs= 5HZ or less) and you have to apply it between sensor and uC.

To address the offset problem, I recommend following the settings described in Application Note AN5444, section 4.6. This section explains how to use the CTRL6 and CTRL7 registers to set a measurement offset compensation. You can also enter the offset value manually.

Regarding the MotionSP library, I recommend that you consult this document:
For best results, you need to use a software HPF (and possibly also a hardware HPF). From the datasheet it is noted that the hardware HPF has a cutoff frequency of 33 Hz, so below 40 Hz you will not get acceptable values.
One possible strategy is to apply a software HPF, perform integration, and then apply additional filtering to improve the results.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.