Skip to main content
KJose.1
Associate II
August 15, 2022
Solved

How the current consumption of ISM330dlc was measured? Is it for SPI or I2C? Are VDD and VDDIO connected during the current consumption measurement?

..

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
August 22, 2022

Hi @KJ.2ose​ ,

The (average) Vdd consumption is measured on the Vdd line with the device configured but not communicating (so, Vdd and VddIO lines can be considered connected together). Since however the SPI/I2C lines are under the VddIO path, if you decouple Vdd and VddIO and you measure the Idd only on the Vdd path, you ill get the same values ad the ones declared in the DS.

The fact is that you can run SPI and I2C in a broad range of frequencies, that directly affects the overall device's power consumption.

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
August 22, 2022

Hi @KJ.2ose​ ,

The (average) Vdd consumption is measured on the Vdd line with the device configured but not communicating (so, Vdd and VddIO lines can be considered connected together). Since however the SPI/I2C lines are under the VddIO path, if you decouple Vdd and VddIO and you measure the Idd only on the Vdd path, you ill get the same values ad the ones declared in the DS.

The fact is that you can run SPI and I2C in a broad range of frequencies, that directly affects the overall device's power consumption.

-Eleon