Skip to main content
SPate.19
Visitor II
April 16, 2019
Question

How may i implement the Harsh Cornering, Harsh Acceleration and Harsh breaking using ST MEMS Lib?

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    April 30, 2019

    Hi, sorry for the delay in the answer. Which device are you using (accelerometer, 6axis...) and which part number? And which is you target application (e.g. is it an automotive application)? You can btw check the X-CUBE-MEMS1 and the related libraries (here). You could in general use the Motion AR library that enables the activity recognition function, but some sensor enables you to develop a Finite State Machine or a Machine Learning to implement the activity recognition. Regards