Skip to main content
Associate
Jul 14, 2026 9:33 AM UTC
Solved

How LPS27HHW pressure sensor can detect the fall of a human being ?

Please support to update how LPS27HHW pressure sensor can detect the fall of a human being.

Andrew Neil
Andrew NeilBest answer
Super User
Jul 15, 2026 5:03 PM UTC

Wearable Fall Detection System Using Barometric Pressure Sensors and Machine Learning

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

3 replies

Andrew Neil
Andrew NeilBest answer
Super User
Jul 15, 2026 5:03 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
GajrajSAuthor
Associate
Jul 16, 2026 3:48 AM UTC

Thank you for support and sharing….

Federica Bossi
ST Technical Moderator
Jul 20, 2026 12:58 PM UTC

Hi ​@GajrajS ,

LPS27HHW is a water-resistant absolute pressure sensor that does not include an embedded fall-detection algorithm. But depending on the specific application and the sensor placement, it could contribute to a fall-detection system since a pressure difference can be converted to an altitude variation.

 

For example, under normal atmospheric conditions near sea level and at ambient temperature (20-28 ºC), it can be approximated that 1 hPa of pressure change corresponds to 8.3 meters of height difference. This is generally valid for small altitude differences (under hundreds of meters).

 

Consider that pressure variation may also be caused by weather changes, doors opening and closing, etc. So the pressure sensor by itself cannot reliably be used for fall-detection. We recommend pairing it with an accelerometer and/or a gyroscope for a more robust fall-detection solution. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.