Skip to main content
nadza
Associate II
November 28, 2022
Question

How I do I2C Connect for the ISM330DHCX sensor

* Initialize the LSM6DSL sensor */

LSM6DSL_Init(&MotionSensor);

/* Configure the LSM6DSL accelerometer (ODR, scale and interrupt) */

LSM6DSL_ACC_SetOutputDataRate(&MotionSensor, 26.0f); /* 26 Hz */

LSM6DSL_ACC_SetFullScale(&MotionSensor, 4); /* [-4000mg; +4000mg] */

LSM6DSL_ACC_Set_INT1_DRDY(&MotionSensor, ENABLE); /* Enable DRDY */

LSM6DSL_ACC_GetAxesRaw(&MotionSensor, &axes); /* Clear DRDY */

this code is used for another gyroscope in the example in the link. I'm trying to use this code for my im330dhcx but these parts are getting errors in CubeIde. How can I solve it? (I am the version I adapted io_ctx . BusType   = ISM330DHCX_I2C_BUS;

 io_ctx . Address   = ISM330DHCX_I2C_ADD_L;

 io_ctx . Init    = HAL_I2C2_Init;

 io_ctx . DeInit   = HAL_I2C_DeInit;

 io_ctx . ReadReg   = HAL_I2C_ReadReg;

 io_ctx. WriteReg  = HAL_I2C2_WriteReg;

 io_ctx . GetTick   = BSP_GetTick;)

This topic has been closed for replies.

2 replies

PST
Associate
December 22, 2022

Hi,

I have the same problem. Have you found a solution?

Best

P