Skip to main content
unternehmen
Associate II
Nov 2, 2019 1:29 PM UTC
Question

How does the ais1120sx work?

About which bits is the CRC for AIS1120sx formed? 8 to 31?

    This topic has been closed for replies.

    3 replies

    Eleon BORLINI
    ST Employee
    Nov 4, 2019 10:22 AM UTC

    Hi @unternehmen​ , AIS1120sx CRC is derived by the value of 32 bits (0 to 31) and results in a 8-bit value that evaluates the transmitted/received data are OK. The 32 CRC-related bits are described at p. 48 and 49 of the datasheet . Basically, the input of the CRC procedure is the 32-bit value previously described, that is divided by the polynomial function described in the datasheet p.48 and, if no error, the output of this division will be an 8-bit value equals to 00h. Regards

    unternehmen
    Associate II
    Nov 10, 2019 2:20 PM UTC

    Hi Eleon,

    that means I have to make a cyclic redundancy check over bit 0 to 7? What does it make sense if I form a crc over eight zeros? Can I not start immediately from bit 8?

    Eleon BORLINI
    ST Employee
    Nov 18, 2019 10:38 AM UTC

    Hi @unternehmen​ , this is the required standard for automotive grade. 32 bits are required to check a series of registers, but the final check can be done on 8-bit. Regards