Skip to main content
Associate
September 4, 2024
Question

How can I manually control the background calibration of my IIS2ICLX-Accelerometer?

hi!
I have a problem with the calibration of the IIS2ICLX-Accelerometer. I see there is happening a calibration but because I make a sensor fusion in the next step, I want to have the calibration fixed once its done. In the data-sheet and the forum I couldnt find a solution. Is there a possibility to manually control the background calibration process?
Thanks!

This topic has been closed for replies.

2 replies

Federica Bossi
ST Technical Moderator
September 9, 2024

Hi @Tim0_ ,

The accelerometer is calibrated at production level, and the calibration values are stored in the reserved registers, and it is not suggested to modify them. You could use a calibration library, such as the MotionAC library: it provides real-time accelerometer calibration through offset and scale factor coefficients used to correct accelerometer data.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Tim0_Author
Associate
September 9, 2024

hi!

Thanks for your kind reply.

I still have the impression that kind of background calibration happens in the firmware. When I start up the sensor, values are grossly off but after few iterations of aligning the different axes to gravity the output data at rest get closer to zero. Am I dreaming? kind regard