Skip to main content
BSeeg
Associate
January 23, 2023
Question

how can i change the STEVAL-MKI109V3 VDDIO to 3.3 V or get the INT1_up or INT2_up signals with an 3.3V Level?

..

    This topic has been closed for replies.

    2 replies

    Peter BENSCH
    ST Technical Moderator
    January 23, 2023

    Welcome, @BSeeg​, to the community!

    you can use the command *setvddio3.3 to set VDDIO=3.3V. This and all other commands are listed in UM2116.

    Hope that helps?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    BSeeg
    BSeegAuthor
    Associate
    January 23, 2023

    Hello Peter

    Is there a way to send comands in the unico Gui?

    I tested The UART Interface and only the command

    "*list"

    did somthing

    the Command

    "*setdbMKI195V1" to select the LSM6DSRX Sensor i use got an

    "inf Adapter nor supported" response

    The conds *setvddio3.3 or *setvdda3.3 changed nothing nor got an response.

    best regards Bene