Skip to main content
CTett.1
Associate II
April 28, 2022
Question

How can I change the SD card in the sensortile.box?

Hi,

I wanted to replace the SD card of the sensortile.box with a faster one, but then I am not able to upload my application. Does anyone know what the problem could be?

Thanks in advance and best regards, Carla

    This topic has been closed for replies.

    7 replies

    niccolò
    ST Employee
    April 29, 2022

    Hi Carla @CTett.1​ ​ ,

    there should not be any problem with faster sd cards

    I don't think that the datalog speed depends on the sd card speed, so I don't recommend to change it.

    anyway, if you want to use that one, try to format it before using it, maybe the firmware is not able to write the flow on the card.

    please, check if there is a DefaultApp.json file in it.

    Niccolò

    CTett.1
    CTett.1Author
    Associate II
    May 2, 2022

    Hi Niccolò @niccolo.ruffini​ ,

    Thanks for the answer, unfortunately formatting the SD card before using it doesn't help. There is no DefaultApp.json file after setting the firmware. What else could be the problem?

    Thanks for your help and best regards,

    Carla

    niccolò
    ST Employee
    May 2, 2022

    Hi Carla @CTett.1​ ,

    let me try to ask you a few question to understand

    1- are you able to read/write the sdcard without using the sensortile.box?

    2- what class and size is the sdcard?

    3- if you upload a new application I imagine that you get an error, but what if you connect to the board? is there the new application running, or the previous one?

    Niccolò

    niccolò
    ST Employee
    May 27, 2022

    Hi Carla,

    sorry for the delay in the answer, the json file is not what I'd expect, I fear that an sdcard of that type is not supported

    can I ask you why do you think the problem in writing speed is due to the sdcard?

    Niccolò