Skip to main content
Associate II
April 24, 2023
Solved

Hi ST support Team, Can you share with us marking code for the PN: ASM330LHHXTR? Many thanks. Danny,

..

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    April 25, 2023

    The marking of the ASM330LHHXTR is LC.

    The groups of digits 213 or 307 stand for the date code in the form YWW, i.e. the last digit of the production year and two digits for the calendar week.

    A digit can only be used to represent the year within a decade, but the ASM330LHHX was only launched in 2022, so 307, for example, represents calendar week 7 in 2023.

    Hope that helps?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    7 replies

    Tesla DeLorean
    Guru
    April 24, 2023

    @Billy OWEN​ please flag to appropriate parties

    Documentation Fail, Marking Codes are a repetitive question

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    DNguy.8Author
    Associate II
    April 25, 2023
    Hi Billy and Tesla,
    Good day,

    The last time we received the part which is marked LC-213.
    Last week when we checked the incoming part we detected it’s LC-307
    Can you explain the difference between LC-213 and LC-307?
    I think that maybe exited another marking code for the PN : ASM330LHHXTR.
    LC-***.
    But we don’t understand their meaning.
    Can you share with us the specification for the marking code of the part
    ASM330LHHXTR or any document which we can follow and no need to make the
    question to you in the future?
    Many thanks.



    Thanks and Best regards
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    April 25, 2023

    The marking of the ASM330LHHXTR is LC.

    The groups of digits 213 or 307 stand for the date code in the form YWW, i.e. the last digit of the production year and two digits for the calendar week.

    A digit can only be used to represent the year within a decade, but the ASM330LHHX was only launched in 2022, so 307, for example, represents calendar week 7 in 2023.

    Hope that helps?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    MPham.2
    Associate
    April 26, 2023

    Hi Peter

    As your mention, PN: ASM330LHHXTR was only lauched in 2022, while our buyer is buying the part with DC 307 (Year 2023, week 07). Could you double check with the production history of this part to ensure we are buying correct part? I'm worry about the Counterfreit in the market.

    Best regards

    Peter BENSCH
    ST Technical Moderator
    April 26, 2023

    "was only lauched in 2022" here means that there was no ASM330LHHXTR before 2022, but only after. And 2023 is after that. ;)

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.