Skip to main content
Rrome.1
Associate
May 5, 2020
Question

Hi, I need the STEVAL MKI022V1 evaluation board software for Windows7, where can I download it? thank you so much for your help.

..

    This topic has been closed for replies.

    4 replies

    Eleon BORLINI
    ST Employee
    May 5, 2020

    Hi @Rrome.1​ , the STEVAL MKI022V1 is a nrnd (no more supported) kit that should be equipped with a dedicated CD with a GUI that runs on Windows XP OS. Did you already tried to install the SW on Win7? Regards

    Rrome.1
    Rrome.1Author
    Associate
    May 6, 2020

    hi,

    yes I tried to install it, the software would seem compatible with W7/64, the problem is the device driver, I assumed that ST in the meantime had developed the driver for 64bit system.

    thanks

    Eleon BORLINI
    ST Employee
    May 6, 2020

    Hi @Rrome.1​ , adding STM32 topic which is fitting more the request. I see that the STEVAL MKI022V1 mounts an ST7 microcontroller and that the related drivers are limited to Win XP OS. You could try to install these USB drivers for ST LINK (STSW-LINK009) and check if it works... Regards

    Rrome.1
    Rrome.1Author
    Associate
    May 8, 2020

    thanks for your answer, I tried the STSW-LINK009 driver but unfortunately it didn't work.