Skip to main content
CMart.11
Visitor II
May 16, 2022
Solved

hi, am i able to use this sensor and programming board: STEVAL-BCN002V1B to create and use apps from the st ble app?

..

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    May 27, 2022

    Hi @CMart.11​ ,

    You should be able to interface the STEVAL-BCN002V1B with the STBLESensor app, but not to use the same app builder of, for example, the Sensortile.box.

    In order to change the parameters here, you should act on the STSW-BLUETILE-DK, which is the is the reference firmware package, or on the BlueST-SDK code.

    How to use the BlueNRG-Tile Bluetooth LE enabled sensor node development kit - User manual (st.com)

    In general however, for this kind of application, I would suggest you to use the Sensortile.box, with which you can create your own app and change the devices ODRs directly from the app GUI.

    -Eleon

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    May 27, 2022

    Hi @CMart.11​ ,

    You should be able to interface the STEVAL-BCN002V1B with the STBLESensor app, but not to use the same app builder of, for example, the Sensortile.box.

    In order to change the parameters here, you should act on the STSW-BLUETILE-DK, which is the is the reference firmware package, or on the BlueST-SDK code.

    How to use the BlueNRG-Tile Bluetooth LE enabled sensor node development kit - User manual (st.com)

    In general however, for this kind of application, I would suggest you to use the Sensortile.box, with which you can create your own app and change the devices ODRs directly from the app GUI.

    -Eleon