Skip to main content
bjha.1
Visitor II
February 15, 2023
Question

Hello Everyone, I am working on the lsm6dsl sensor from two week and i read the data sheet but I can't find the Suitable answer about my question. My question is to set threshold for x y and z axis. if the tilt greater than 30 generate interrupt.

can anyone provide answer.

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
April 12, 2023

Hi @bjha.1​ ,

Welcome to ST Community!

Have a look at AN5040.

If you are referring to the 6D orientation detection, you can't set a threshold values of 30 degrees but you need to choose another one from the values given in the table 27 page 39.

Otherwise, if you refer to absolute wrist tilt, the threshold parameter can be configured through the embedded functions register A_WRIST_TILT_THS by setting the WRIST_TILT_THS field as described in page 55 of AN5040.

Note that the default value of register 54h is 500 mg, corresponding to a tilt angle of 30 degrees.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.