Skip to main content
YBend.1
Associate III
March 21, 2022
Solved

Hello all !! I needed to use a push pull type capacitive accelerometer for an application in my organisation. Can someone please share a few ST electronics MEMS capacitive accelerometer ICs based on push pull type sensing. Range preferably 10g-100g.

..

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    March 25, 2022

    Hi @YBend.1​ ,

    please note that ST MEMS accelerometer are capacitive ICs, not based on push pull sensing but on a different technology, i.e. interdigitated fingers.

    I can however suggest a device capable of sensitivity up to 10g-100g, such as the H3LIS331DL, a low-power high performance 3-axis linear accelerometer with dynamically user selectable full scales of ±100g/±200g/±400g and capable of measuring accelerations with output data rates from 0.5 Hz to 1 kHz.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

    -Eleon

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    March 25, 2022

    Hi @YBend.1​ ,

    please note that ST MEMS accelerometer are capacitive ICs, not based on push pull sensing but on a different technology, i.e. interdigitated fingers.

    I can however suggest a device capable of sensitivity up to 10g-100g, such as the H3LIS331DL, a low-power high performance 3-axis linear accelerometer with dynamically user selectable full scales of ±100g/±200g/±400g and capable of measuring accelerations with output data rates from 0.5 Hz to 1 kHz.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

    -Eleon

    YBend.1
    YBend.1Author
    Associate III
    April 18, 2022

    Thanks a lot Eleon.