Skip to main content
Kattinti Siva Krishna
Associate II
January 8, 2018
Question

H3LIS331DL

  • January 8, 2018
  • 3 replies
  • 906 views
Posted on January 08, 2018 at 15:19

Dear Team,

I am trying to configure CTRL_REG4 of H3LIS331DL chip register value multiple times with default configuration, which is creating a problem of not generating data ready interrupt. If I am not configuring it then working fine.

Could any one please tell me what went wrong or did I made configuration as wrong or Accel chip itself internally having the mechanism of if we configure CTRL_REG4 with multiple time default value then Data Ready Interrupt will not generate? Please help us finding on this.

Thanks,

Siva.

#h3lis331dl #h3lis331dl-data-ready-interrupt #h3lis331dl-configuration
This topic has been closed for replies.

3 replies

ST Employee
January 8, 2018
Posted on January 08, 2018 at 16:17

Can please specify which value are you writing to the CTRL_REG4 and also tell me how many times you write it there.

I can then try to reproduce your issue.

But I think the problem is somewhere else, you can write to the register how many times you want.

Kattinti Siva Krishna
Associate II
January 8, 2018
Posted on January 08, 2018 at 17:17

Dear Miroslav,

Thanks for your reply.

Sequence will be as follows :

Power On,

Configure CTRL_REG1

I am writing the following settings to the CTRL_REG4

.BDU = 0

.BLE=0

.FS1&FS0=0&0

.SIM=0

To reproduce the issue, Please write this values into the CTRL_REG4 and Rotate the sensor.

I am not able to reproduce the issue if accel sensor is in idle. But able to reproduce the issue, if I am rotating or shacking with my hand. This configuration I am making while sensor is rotating.

100 times I am writing into the register.

Please let us know what might be the root cause.

Thanks,

Siva.

.

ST Employee
January 8, 2018
Posted on January 08, 2018 at 18:43

Why do you write the configuration so many times?

Cannot it be a problem with hardware connection?