Skip to main content
Waqas Ahmad
Associate
March 20, 2017
Question

H3LIS200DL I2C not working for more than 5 mins

Posted on March 20, 2017 at 13:40

Hi, I am using H3LIS200DL with RFduino (RFD22102 ) as microntroller, I have used the schematic given in data sheet except I have connected CS pin to Vdd (for using I2C). Also I am using Arduino H3LIS331Dl_demo code attached below.

The IC works fine for 5mins and then readings become constant. And when I use it again after 10 hours or so, it again works fine for 5mins only. This is happening from 3 days. I have also resoldered it and rechecked the capacitors. 

I used 3 ICs. One worked fine but the same problem is happening with other 2.

Is this any soldering problem?

Am I missing any point?

Help would be appreciated.

H3LIS200Dl data sheet : 

http://www.st.com/content/ccc/resource/technical/document/datasheet/6c/e1/2a/9d/29/58/4e/25/DM00162194.pdf/files/DM00162…

 

RFD22102 data sheet:

http://www.st.com/content/ccc/resource/technical/document/datasheet/6c/e1/2a/9d/29/58/4e/25/DM00162194.pdf/files/DM00162…

This topic has been closed for replies.