Skip to main content
MMaie.1
Associate
May 14, 2020 12:16 PM UTC
Solved

Get factory settings/ firmware of the STEVAL-BCN002V1B

Hello,

I have a question to the STEVAL-BCN002V1B.

I try some BLE-Examples and flash the bord with some firmware example from the SDK.

Now I can't pair the board with my mobile phone ST APP. Which firmware do I have to use to get the default factory settings back.

Thanks a lot for your support.

Cheers Max

    This topic has been closed for replies.
    MMaie.1
    MMaie.1Best answer
    Associate
    May 14, 2020 1:01 PM UTC

    Oh now it works.

    I used the BLE_SensorDemo_Use_OTA_ServiceManager.hex file

    2 replies

    MMaie.1
    MMaie.1AuthorBest answer
    Associate
    May 14, 2020 1:01 PM UTC

    Oh now it works.

    I used the BLE_SensorDemo_Use_OTA_ServiceManager.hex file

    Eleon BORLINI
    ST Employee
    May 14, 2020 1:05 PM UTC

    Hi @MMaie.1​ , you can first try to interface the BCN002V1B with Unicleo-GUI, to check the BLE connectivity on a device that can run Unicleo and is provided by a BLE module. Or, alternatively, you can use the STBLESensor app on your smartphone. To "get back" to a factory tested FW I suggest you to flash an original BLE example such as the BLE_SensorDemo.bin file, that you can find in the\Firmware\BLE_Examples folder of the STSW-BLUENRG1-DK. For this purpose ou can use an ST-LINK/V2 programmer and the STM32Cube Programmer. Regards