Skip to main content
Dmitry Vasilenko
Visitor II
Oct 13, 2020 11:43 AM UTC
Solved

Gadget position sensor

Hi, 

our customer is in search for a economical solution for a gadget posistion sensor, that senses 2 positions: the gadget is in standing or in laying positions. What can we suggest?

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Oct 13, 2020 1:08 PM UTC

Hi @Dmitry Vasilenko​ ,

Since the target application is a gadget, I believe it should consume as little power as possible. So, I would suggest the LIS2DW12 ultra-low-power high-performance three-axis linear accelerometer, which has the embedded 6D/4D orientation digital feature, described in the datasheet and in the AN5038 application note at p. 23.

You can also refer to the C example repository on Github for the code implementation of this feature --> lis2dw12_orientation.c.

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Oct 13, 2020 1:08 PM UTC

Hi @Dmitry Vasilenko​ ,

Since the target application is a gadget, I believe it should consume as little power as possible. So, I would suggest the LIS2DW12 ultra-low-power high-performance three-axis linear accelerometer, which has the embedded 6D/4D orientation digital feature, described in the datasheet and in the AN5038 application note at p. 23.

You can also refer to the C example repository on Github for the code implementation of this feature --> lis2dw12_orientation.c.

-Eleon