Skip to main content
PWeil.2
Visitor II
December 27, 2022
Question

For X-NUCLEO-IKSO1A3 and NUCLEO-L476RG only options IKSO1A1 and IKSO1A2 which are working well but not option IKSO1A3 with STM32CubeExpansion_MEMS1_V4.4.1

in order to get all sensor working

This topic has been closed for replies.

1 reply

ST Technical Moderator
January 10, 2023

Hello @PWeil.2​,

You are right, the X-CUBE-MEMS1 expansion package version 4.4.1 supported the STM32L476RG devices and NUCLEO-L476RG board with X-NUCLEO-IKS01A1 and X-NUCLEO-IKS01A2 Boards.

You can check this history and main changes in the "Release notes" file of the package.

Note that the NUCLEO-L476RG examples and applications are replaced by NUCLEO-U575ZI-Q ones, since the release V9.3.0 of X-CUBE-MEMS1 expansion package.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks