Skip to main content
A. L.
Associate
Sep 2, 2017 3:29 AM UTC
Question

''Fluctuating'' acceleration output with LIS3DH

Posted on September 02, 2017 at 05:29

Hi there, I am currently running 4 LIS3DH chips in SPI configuration, outputting accel data @ 12bit (high res) 200Hz, +/- 2gs configuration.

The chips are not moving, and I noticed from the serial output terminal that the x,y,z acceleration value fluctuates in random intervals. The fluctuation applies throughout all of the LIS3DH chips, and is consistently scaled (up/down) by 2 on all acceleration axes output, in the same set of readings.

(e.g. x:1.01 y:-0.06 z:9.50m/s^2 fluctuates to x:2.09 y:-0.25 z:19.08m/s^2 in the next data set).

The raw value seems have this pattern of fluctuation as well (scaled by 2). (e.g. z raw: 15936 to 31424).  

The code I am using can be found at 

https://github.com/adafruit/Adafruit_LIS3DH

 (Adafruit_LIS3DH.cpp). 

Am I missing something? Thank you.

#outputs #lis3dh #fluctuates
This topic has been closed for replies.

1 reply

A. L.
A. L.Author
Associate
Oct 21, 2017 12:31 AM UTC
Posted on October 21, 2017 at 02:31

Anyone have anything similar, or any experience on resolving this?