Skip to main content
TWang.12
Visitor II
May 10, 2022
Question

Failed to access LIS2DH12 motion sensor WHO_AM_I register via MCU STM32F412CEUx (UFQFPN48).

PB3 and PB10 are enabled as I2C2_SDA and I2C2_SCL to connect to LIS2DH12 SDA and SCL, the i2c2 code is generated in STM32CubeIDE v1.6.1.

PB3 and PB10 have pull-up resistors.

LIS2DH12 CS and SD0 are connected to Power Supply 3.3V. The address for it is right shifted 1 bit to 0x19.

The code is generated as the following.

main.c

int main(void)

{

...

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_I2C2_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

...

}

/**

 * @brief I2C2 Initialization Function

 * @param None

 * @retval None

 */

static void MX_I2C2_Init(void)

{

 /* USER CODE BEGIN I2C2_Init 0 */

 /* USER CODE END I2C2_Init 0 */

 /* USER CODE BEGIN I2C2_Init 1 */

 /* USER CODE END I2C2_Init 1 */

 hi2c2.Instance = I2C2;

 hi2c2.Init.ClockSpeed = 100000;

 hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_2;

 hi2c2.Init.OwnAddress1 = 0;

 hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

 hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

 hi2c2.Init.OwnAddress2 = 0;

 hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

 hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

 if (HAL_I2C_Init(&hi2c2) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN I2C2_Init 2 */

 /* USER CODE END I2C2_Init 2 */

}

stm32f4xx_hal_msp.c

/**

* @brief I2C MSP Initialization

* This function configures the hardware resources used in this example

* @param hi2c: I2C handle pointer

* @retval None

*/

void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 if(hi2c->Instance==I2C2)

 {

 /* USER CODE BEGIN I2C2_MspInit 0 */

 /* USER CODE END I2C2_MspInit 0 */

  __HAL_RCC_GPIOB_CLK_ENABLE();

  /**I2C2 GPIO Configuration

  PB10   ------> I2C2_SCL

  PB3   ------> I2C2_SDA

  */

  GPIO_InitStruct.Pin = GPIO_PIN_10;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;

  GPIO_InitStruct.Pull = GPIO_PULLUP;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF4_I2C2;

  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = GPIO_PIN_3;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;

  GPIO_InitStruct.Pull = GPIO_PULLUP;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF9_I2C2;

  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  /* Peripheral clock enable */

  __HAL_RCC_I2C2_CLK_ENABLE();

 /* USER CODE BEGIN I2C2_MspInit 1 */

 /* USER CODE END I2C2_MspInit 1 */

 }

}

However, when issuing the command to access LIS2DH12 WHO_AM_I register. It always return HAL_ERROR.

+extern I2C_HandleTypeDef hi2c2;

+ REG_FN(f_sensorid)

+{

+  // I2C Debug Start

+#define LIS2DH12_ADDR 0x19

+#define WHO_AM_I    0x0f

+  uint8_t buf = WHO_AM_I;

+  uint8_t ID;

+  HAL_StatusTypeDef ret;

+

+  // Tell LIS2DH12 that we want to read from the WHOAMI register

+  ret = HAL_I2C_Master_Transmit(&hi2c2, LIS2DH12_ADDR, &buf, 1, 1000);

+  if ( ret != HAL_OK ) {

+    uart_printf("Error Tx\r\n");

+  } else {

+

+   // Read 2 bytes from the temperature register

+   ret = HAL_I2C_Master_Receive(&hi2c2, LIS2DH12_ADDR, &ID, 1, 1000);

+   if (ret != HAL_OK ) {

+    uart_printf("Error Rx\r\n");

+   } else {

+

+    //Combine the bytes

+    //HAL_I2C_Mem_Read(&hi2c2, LIS2DH12_ADDR, WHO_AM_I, 1U, &ID, 1U, 1000);

+        uart_printf("WHO AM I: %02x\r\n", ID);

+   }

+  }

+#endif

+  // I2C Debug End

This topic has been closed for replies.