Skip to main content
anthony2
Associate
November 27, 2013
Question

Example for LSM303DLHC Accelerometer

Posted on November 27, 2013 at 15:26

Hi,

I need to read the accelerometer data from LSM303DLHC. I use the STM32F401 Discovery board and the ''stm32f401_discovery_lsm303dlhc.c'' library.

I read carefully the datasheet, especially the section 7.1 in page 24 with the register setup but I would like to know if someone has any project example that could help me to understand how to use the sensor.

Thank you in advance.

Kind regards,

Antho

This topic has been closed for replies.

6 replies

Thiago REIS
Associate II
November 27, 2013
Posted on November 27, 2013 at 17:01

Hello Antho,

We are currently creating a section of this forum to contain examples of applications using ST's MEMS. I will add one example for you application too.

Once we have the codes, I can also post it here as a reference.

Thank you very much,

Thiago Reis

anthony2
anthony2Author
Associate
November 28, 2013
Posted on November 28, 2013 at 09:41

Hi Thiago,

Thank you for your time. I think that this new section is a good idea, it might be very helpful for beginners like me.

Antho

olavi
Associate II
December 16, 2013
Posted on December 16, 2013 at 06:31

Antho,

Just in case that you are still looking some additional information about the LSM303 usage, I would recommend that you look the selftest.c file in the F401 demonstration folder.  There you have the code to read the sensor data (such as LSM303DHLC_CompassReadAcc) using the I2C connection.  Once you have the accelerometer and compass data, you should combine that with the gyro data (from L3GD20).

The accelerometer has a lot of short term noise, but good long term stability.  The gyro has little noise, but it has a bad drift.  You can use a Kalman filter to combine the data streams, simple low pass and high pass filters, or add-hoc methods (such as model based bias adjustment).

sudhi
Visitor II
December 20, 2013
Posted on December 20, 2013 at 01:23

Hi Thiago,

Good to know that you are adding a separate section for the applications.

The link

http://www.st.com/web/en/catalog/tools/PF257534#

anthony2
anthony2Author
Associate
January 8, 2014
Posted on January 08, 2014 at 17:49

Hi,

Thanks for your time Ollie, your reply has been very helpful.

Actually, I am trying to test the accuracy of the Inertial Measurement Unit for a school project. That is why I need to get the output data from both the accelerometer and the gyroscope.

But first, I am trying to exploit the output data to turn on the LED matching with the acceleration direction (as in the demo of the gyroscope). I set the linear acceleration range at 8g in the register but I have not been able to determine which kind of data is returned by the function ''LSM303DLHC_Read(ACC_I2C_ADDRESS,LSM303DLHC_OUT_X_L_A,6,tmpbuffer)''.

In the data sheet, it is mentioned that the 16 bit data output is expressed in 2's complement. this data is then converted into a float. The buffer declaration is : float buffer[6]. However, in the different programs I read, the X and Y values were define by Xval = buffer[0] and Yval = buffer[1] or buffer[2].

But, aren't we supposed to get only the Xval by the function above (parameter : LSM303DLHC_OUT_X_L_A) ? And why is the float value converted in 8 bit for the test (''if((int8_t)Buffer[0] < -2)'') ?

About the data filtering, I will look into the Kalman filter, thank you for the idea.

Kind regards,

Antho
Thiago REIS
Associate II
January 17, 2014
Posted on January 17, 2014 at 13:33

Hello Sudhi,

Were you able to download the software that you needed?

If not, please send me a message with your contact information and project description at thiago.reis@st.com

Thank you,

Thiago