Skip to main content
Associate
Oct 16, 2025 1:28 AM UTC
Question

ESP32 deep-sleep with LSM6DSOX step-detector: how do you cut false wakes?

I’m building a small wearable logger: ESP32 sleeps most of the time, wakes on LSM6DSOX step-detector, logs, then goes back to sleep. Looking for settings that work in practice:

  • ODR/FS and step-detector config that avoids vibration false wakes

  • INT wiring to an RTC-capable GPIO (pull-up value?), latched vs pulsed INT

  • FIFO vs direct interrupt; simple debounce in firmware

  • Re-init after deep-sleep (soft reset, clear INT, reprogram registers)

  • Typical deep-sleep current numbers with the IMU powered vs fully off

Concrete numbers welcome (thresholds, durations, current, wake frequency). Thanks!

This topic has been closed for replies.

2 replies

gtrkingAuthor
Associate
Oct 18, 2025 5:17 AM UTC

Update: first pass is working better.

  • LSM6DSOX: ODR 26 Hz, FS ±4 g, step-detector ON, threshold = 2

  • INT1 → RTC GPIO with 10 kΩ pull-up; added 400 ms cool-down in firmware

  • Deep-sleep sits around ~9–12 µA at 3V3; false wakes dropped a lot

Hardware reference (external): the board I used is ESP32-WROOM.
If you’ve reached <8 µA with similar wiring, what changed it for you?

Federica Bossi
ST Technical Moderator
Oct 20, 2025 12:56 PM UTC

Hi @gtrking,

Lower ODRs reduce power but may miss steps or increase latency. 26Hz could be a good compromise. You can experiment with thresholds 2–4 depending on your environment and motion profile.

FS ±4 g is a balanced choice for wearables, but you could try also ±8g.

Use latched interrupt mode if available (interrupt stays asserted until cleared) to avoid missing events during ESP32 wake-up latency.

In addition, you can disable unused sensor features (e.g., FIFO if not needed).

Ensure sensor is in low-power mode when idle.

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.