Skip to main content
Associate III
Jun 30, 2026 12:36 AM UTC
Question

Electrical Signal

On a garage floor a small limestone block 150 mm by 50 mm by 20 mm on a fixed roller support 

XXXXXXXXXXXXXA
F              R

Sensor at A, the F and R are small wooden blocks and a roller.  

I pick up the electrical signal to 420 Hz.  

The limestone is vibrating at 460 Hz quite nicely as it is a heavily degraded block so the Sensor TileBox Pro is quite good, but should I normally see electrical signals this high, the CX1 stops at about 180.